STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

scroll list add and remove elements

Hi,I want to create a scroll List where the elements have to be added or removed. I tried using remove but not able to remove elements even through call back like scroll list.is there solution?or how can I use remove ?Thankyou,

Revanth by Associate III
  • 2048 Views
  • 2 replies
  • 0 kudos

Resolved! Text resources are invisible while in the simulation?

ProblemWhen running the simulation, the text resources are invisible. Additional notes:Q: Is the resource properly configured? A: Yes. I think so. Here's an example of the PressureString:Q: Is the simulator Locale configured to GB?A: Yes. I think so....

0693W00000GXQ28QAH.png 0693W00000GXQ6oQAH.png 0693W00000GXQ4TQAX.png 0693W00000GXQ7IQAX.png
GBert.2 by Senior
  • 5223 Views
  • 11 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.