STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

X-CUBE-TOUCHGFX 4.18.0 is out

4.18.0 was released 20th of October.Release notes (which can be found here: https://support.touchgfx.com/docs/miscellaneous/changelog) is as follows:New TouchGFX Designer Features:New Widget: Video.Added support for new .xml text database.Removed Tex...

HP by Senior III
  • 8693 Views
  • 16 replies
  • 1 kudos

How to include main.c in the Screen1View.cpp?

Hello :)I'm trying to include main.c into Screen1View.cpp but I do not have any idea how to do it.I need to use array of 64 elements from main file into Screen1View file (the array is called current_temp).Does anyone have any idea how to do it? If so...

0693W00000GZOdGQAX.png
AWe.1 by Associate II
  • 1699 Views
  • 2 replies
  • 0 kudos

(STM32H750 + SDRAM + NAND flash) => display stuck

Hello, I used a 32MB SDRAM and a 1GB NAND flash, the size of LCD is 480 * 800, the images save as RGB888 and ARGB8888 format. The images data must copy from NAND to SDRAM when used. I read all images data one screen used in setupScreen function whe...

V.H by Senior
  • 675 Views
  • 0 replies
  • 0 kudos

Resolved! LCD connected to STM32f429 does not work

Hello,I am using STM32F429BI.I use CubeIDE 1.7.0 and CubeMX. I use touchGFX 4.16.1 as a graphic tool.The LCD specification used is attached as a file.​LTDC is set up like the attached image  My question is1. Are there any wrong LTDC settings?2. Do I ...

0693W00000GYWMQQA5.png 0693W00000GYWMVQA5.png 0693W00000GYWMGQA5.png
Hwoo- by Associate II
  • 3129 Views
  • 4 replies
  • 0 kudos

Compile error in Windows 11

I need a help or guide.I have a problem with TouchGFX.I updated Windows to Windows 11 recently.I can't compile it after it is updated.This is my error message.Run Simulator  Generate    Done  Generate Assets    make -f simulator/gcc/Makefile assets -...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.