STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! SBSFU | KMS and X509 support | RAM usage by SE

Hello all,Quick question. Why does Secure Engine (SE) consume so much RAM for projects supporting KMS and X509? In sample projects, by default it's around 120 [kB] of RAM assigned for SE. For purely "building" purposes we decreased it down to 36 [kB]...

Key Storage feature - STSAFE-A110

Hi all,I was hoping someone could advise me on the key storage feature of the part number STSAFE-A110 (STSAFA110S8SPL02).We have a device in the market-place at present which is currently undergoing a redesign. The device itself is a network security...

RDP regression - OEMKEY1 and OEMKEY2

Hello, What is the status of the OEMKEY1 and OEMKEY2  when the RDP regression happens. Are those keys are also erased ?  Thanks in advance.Best Regards,Surya S

Surya S by Associate II
  • 2003 Views
  • 2 replies
  • 2 kudos

Resolved! H753 Target not found after security option byte

Hey,I tried to activate the HDP feature / secure software area on H753 following this documentation HDP secure area for STM32H7B3xx microcontrollers - Application note. I did only activate the security option byte not the secure software area itself....

Resolved! Error when writing secure firmware image to STM32U535

I followed the secure image tutorials as can be seen in AN4992/AN5054  or in videos made available by ST. The process takes place without errors, as can be seen in the images below (start address is 0x08000000).Smart card is valid and working:However...

MarceloBarros_0-1706993166340.png MarceloBarros_1-1706993188848.png MarceloBarros_2-1706993221867.png

Firmware MPU configuration and SBSFU FPU exceptions

It seems to be a recurring challenge in the community posts of getting firmware MPU configuration to work with SBSFU. We also had the problem of application firmware hanging when running it with SBSFU. A solution of clearing floating point unit flags...

sute by Associate III
  • 3395 Views
  • 5 replies
  • 0 kudos

How to exit safe mode for STM32H735.

How to exit safe mode when the security position of the chip is 1 and the protection area of the flash of the new chip is from 0x080000000 to 0x082020000, but the content in the flash is erased,Thank you.

wux by Associate
  • 1905 Views
  • 2 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.