2024-02-15 7:49 AM - edited 2024-02-15 8:21 AM
Hi all,
I was hoping someone could advise me on the key storage feature of the part number STSAFE-A110 (STSAFA110S8SPL02).
We have a device in the market-place at present which is currently undergoing a redesign. The device itself is a network security orientated product, to which we would like to add en/decryption.
In order to ensure our device can be updated in the field, and during the process of development, we were hoping the 16-slot secure key storage fields that the ATSAFE-A110 offers, would be a rewritable area of memory, or is this memory bank one-time-programmable (OTP) only?
Should the key storage only be OTP; can this device be used to encrypt/decrypt data when provided with a key from an MCU, to lessen the processing load of the MCU?
Or does ST offer any devices that could perform such a role?
Many thanks for taking the time to read this, and kind regards,
Josh.
2024-02-19 8:49 AM
Hi @JoshHomerston ,
Thanks for the interest of the STSAFE-A110 product.
With STSAFE-A110, the symmetric use case is limited to the key storage with the Local Envelop method.
In that case, the keys are secured by STSAFE-A110 but used by the MCU for encryption/decryption.
For the time being, the only secure element that allow to do such operation is TPM product ST33KTPM2X
Best Regards,
Benjamin
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.