| Subject | Author | Posted | |
|---|---|---|---|
|
I am currently working with SBSFU on the STM32H743ZIT6 series and have implemented several modif...
| 2026-06-07 11:40 PM | ||
|
Hello, STM32H533 It seems that Option Bytes are not programmed during SFI ?? To keep things s...
| 2026-06-04 8:07 AM | ||
|
Hello everyone, I am looking into using HDPL and would like to know if there is any way to comm...
| 2026-06-03 7:09 AM | ||
|
Hello everyone, I am currently working with the Aliro software expansion for STM32Cube using the ...
| 2026-05-20 1:15 AM | ||
|
Hello, I'm currently integrating the SBSFU 2.8 for one of our board, that use a STM32H753, with a ...
| 2026-05-13 7:39 AM | ||
|
Hello,
I've recently managed to modify the SBSFU example for the STM32F413H-Discovery board and a...
| 2026-05-12 7:59 AM | ||
|
Hello, long time lurker, now with an issue that I would like to solve. I developed a firmware ...
| 2026-05-11 3:09 AM | ||
|
Hi, I am working with the OEMiRoT reference project (STM32U385) and I need to configure a singl...
| 2026-05-11 12:51 AM | ||
|
Hello ST Community,
I am working with an STM32U585 custom board and I would like to clarify the...
| 2026-05-07 6:13 AM | ||
|
Hello ST Community, I am working on the NUCLEO-N657X0-Q board with a TrustZone project configured ...
| 2026-05-05 5:16 AM | ||
|
Hello ST Community, I am working on the NUCLEO-N657X0-Q board with a TrustZone project configured ...
| 2026-05-02 8:23 AM | ||
|
Hello everyone. I'm novice in cryptografic, I'm developing a project with STM32H7. I have a file...
| 2026-04-13 11:48 PM | ||
|
Hi, I’m working with the STM32H7S7L86H and using the SAES peripheral to encrypt and decrypt da...
| 2026-04-06 7:42 AM | ||
|
Hello, After spending several days investigating this topic and reviewing all the documentation I ...
| 2026-04-01 9:38 AM | ||
|
In OEMiROT_Boot/Src/low_level_ext_flash.c, function Ext_Flash_EraseSector(), a call is made to EXT...
| 2026-03-11 6:44 AM | ||
|
Suppose I want to implement firmware for STM32U3 without TZ enabled and without the use of GTZC, th...
| 2026-03-04 7:10 AM | ||
|
I read UM3451 (STM32N6xx security guidance for SESIP level 3 certification) chapter 3.2.2 Secure in...
| 2026-03-03 7:00 AM | ||
|
I created a sample project using the STM32N657-DK, but when I try to debug using ST-LINK, each pr...
| 2026-02-26 6:04 PM | ||
|
In STM32Cube_FW_H7RS_V1.3.0, file Projects/STM32H7S78-DK/Applications/ROT/STiROT_iLoader/STM32CubeI...
| 2026-02-06 9:47 AM | ||
|
Hello, After creating a new project based on the FreeRTOS_Queues_ThreadFlags_TrustZone example fro...
| 2025-12-17 4:39 AM |