STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H750IB How set the RDP Level ?

When I set the RDP Level 1 the Controller stops working.I must unpower the Controller and power it agin, NRST didn't work.I use the code:       HAL_FLASH_Unlock();       HAL_FLASH_OB_Unlock();       OBIni.OptionType = OPTIONBYTE_RDP;       OBIni.RDPL...

JFieb.1 by Associate
  • 1906 Views
  • 1 replies
  • 0 kudos

How to repartition SRAM while using trust zone

I am using the SBSFU example of "NUCLEO-L552ZE-Q" Projects.I have added my application code to the NON-Secure application project.When I see "Region_defs.h", in which nonsecure (NS_TOTAL_RAM_SIZE ) size is 192 KB whereas secure (S_TOTAL_RAM_SIZE)size...

PYada.1 by Associate III
  • 2188 Views
  • 2 replies
  • 0 kudos

Resolved! Do STM32F769I - DISCO has any security features?

I was searching for the security features of STM32F769I - DISCO and came to know that only STM32F77x has CRYP and HASH in the STM32F7xx series.Do STM32F769I - DISCO really have security features? If so, can you provide a relevant document regarding t...

MdFayaz by Associate III
  • 1827 Views
  • 3 replies
  • 0 kudos

Resolved! Accidental MCU/Flash write lock up: My misuse or CubeProg bug?

While programming OptionBytes or FW on STM32WLx5 most of the time is OK.In CubeProg I have noticed, that on some MCUs, when I get reading of RDP 0xFF or 0, the next action to program something write related, it could not be done and it's failed.Stati...

ZSvet.1 by Associate II
  • 3332 Views
  • 4 replies
  • 0 kudos

Resolved! STM32CubeU5: how to build TFM applications?

hi all,I would like to experiment with the TFM applications contained in the STM32CubeU5 package on my B-U585I-IOT02A boardunfortunately, it seems that STM32CubeIDE is not supporteddoes anyone have suggestions on how to build the TFM applications, ba...

GTort.1 by Associate II
  • 4351 Views
  • 4 replies
  • 0 kudos

What is the STM32 Programmer CLI CRC calc polynomial?

Hey, I went through the manual of the STM Programmer command line interface and implemented a post build CRC calc with the Safety lib command -sl.C:\PROGRA~1\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin\STM32_Programmer_CLI.exe -sl MESOL_CAN_...

AndreM by Associate
  • 3940 Views
  • 4 replies
  • 0 kudos

Custom loader for SBSFU / STM32WB5MMG - how to run FUS?

I am building a custom loader for SBSFU on the STM32WB5MMG. The loader is similar to the BLE_Ota loader, but instead of using BLE, it loads firmware/wireless stack from an onboard microSD card, as well as being able to write CKS keys.I do need to hav...

crwper by Senior
  • 2832 Views
  • 4 replies
  • 0 kudos

Resolved! How to unlock STM32H5 Flash?

I set my flash OB to iROT-Provisioned (Dont know exactly Product life cycle state, but I can not debug anymore) Based on my understanding, it may be in a CLOSED state. However, I am not sure how to change the state as I want to follow the Debug authe...

HNguy.27 by Associate II
  • 4769 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.