2023-03-13 7:22 AM
When I set the RDP Level 1 the Controller stops working.
I must unpower the Controller and power it agin, NRST didn't work.
I use the code:
HAL_FLASH_Unlock();
HAL_FLASH_OB_Unlock();
OBIni.OptionType = OPTIONBYTE_RDP;
OBIni.RDPLevel = OB_RDP_LEVEL_1;
if ( HAL_FLASHEx_OBProgram(&OBIni) != HAL_OK )
{
HAL_FLASH_OB_Lock();
HAL_FLASH_Lock();
return;
}
HAL_FLASH_OB_Launch();
/* We should not make it past the Launch, so lock
* flash memory and return an error from function
*/
HAL_FLASH_OB_Lock();
HAL_FLASH_Lock();
What must I do, that the controller didnt stop after the HAL_FLASH_OB_Launch(); ?
2023-04-13 8:32 AM
Hello @Jürgen Fiebig,
Check this article How to program STM32 Option Bytes with the HAL API 2. Setting RDP Level
Note: HAL_FLASH_OB_Launch(); is called to generate System Reset to load the new option byte values.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.