2023-03-20 10:24 AM
As I understand OTFDEC will be used to on-fly decryption, while execution (am I correct)?
After debug is fused (RDP set to level 2) all DHUK keys are individual for each device, while during debug phase all keys are common. How can I make test run of the software in production environment with production keys?
2023-04-03 5:20 AM
Hello @VTver.1 ,
Welcome on the Community!
In fact, the embedded OTFDEC decrypts in real-time the encrypted content.
Actually, DHUK has its production value when RDP>0. So, I believe you can run test in RDP1 if you need production keys. The SAES peripheral can wrap (encrypt) and unwrap (decrypt) application keys using these hardware-secret keys DHUK, XOR-ed or not with the application key BHK. You 'll find more details here.
Note that the SAES IP will behave exactly the same whatever the RDP level.
Does that help ? If yes, you can mentioned "best answer" for this comment.
Regards
Pierre
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.