2023-08-16 7:09 AM - edited 2023-08-19 12:08 PM
Hello All,
Do you support all UVC versions on UsbX Azure RTOS running on STM32H735XGT6? Or do you have some restrictions?
Best regards,
2023-08-25 2:20 AM
Hi @mcBe USBX stack support UVC class version 1.5 and there is no limitation you ca generate your project with cubemx and x-cube-azrtos-h7 pack. actually our generated descriptor support MJPEG and UNCOMPRESSED format
You can also refer to this sample application running on STM32H723-nucleo and easily to port to stm32H735
2024-05-22 11:32 PM - edited 2024-05-24 1:17 AM
Hi,
is it possible to use/activate 3 isochronous transactions per microframe?
/* High speed Isochronous Endpoint: MULT setting.*/
#define UVC_ISO_EP_HS_MULT (2 << 3)
Edit: Found the Problem. I needed to increase the amount of send bytes to force the processor to send 3 transactions:
USBD_LL_Transmit(pdev, (uint8_t)(epnum | 0x80U), (uint8_t *)TxPtr, AmountOfSendBytes);
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.