2026-04-30 3:42 AM
I am working with the STM32L4S5VIT6 and currently facing an issue while trying to communicate with the system bootloader over USART. I am using the B-L4S5I-IOT01A Discovery board, on which I am attempting this setup. I have configured BOOT0 correctly and verified that the MCU enters boot mode (the application stops running as expected). I connected USART2 on PA2 (TX) and PA3 (RX), tried swapping TX/RX lines, and also interfaced through a MAX3223 level shifter to a MOXA device, but the STM32CubeProgrammer still reports a “KO – device not responding” error. I have confirmed that the MCU runs user code correctly (LED blink test), so basic functionality is intact. At this point, I suspect either a configuration misunderstanding from AN2606, incorrect peripheral mapping for this specific MCU, or a hardware-level issue with the UART path. Has anyone faced a similar issue with STM32L4 series bootloader communication, or can help clarify the exact USART instances/pins supported in boot mode for this device?
Regards,
~av
Solved! Go to Solution.
2026-05-02 7:14 AM
according to AN2606, you need to check the boot0 pin, the nBoot1 and nBoot0_SW option byte
2026-05-02 7:14 AM
according to AN2606, you need to check the boot0 pin, the nBoot1 and nBoot0_SW option byte
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.