2009-01-03 8:47 AM
STM32F103 and ILI9320 QTFT display
2011-05-17 4:36 AM
Hi tkjmail,
I'm trying to display images on the LCD screen (ILI9329) using an STM32F103ZET6, the problem that I couldn't display colored pictures, I used the ''LCD_WriteBMP function'' for that and I tried with monochrome pictures and it worked well using the ''LCD_DrawMonoBMP function'' which is provided for displaying monochrome BMPs.(these functions are from the demo's in the STonline) Actually, I convert the images into an hex code using a software called the Hex Workshop then I put the image as a const like this for example: const unsigned char IMAGE[] :{ 0x00, 0xFF, 0xFF, 0x00, 0xFF, 0xFF, 0x00, 0xFF, 0xFF, 0x00, 0xFF, 0xFF, 0x00, 0xFF, 0xFF, 0x00, 0xFF, 0xFF, }; an then in the call of the function : LCD_WriteBMP((u32) IMAGE); // if it's a colored picture //LCD_DrawMonoBMP((u32) IMAGE); // if it's a monochrome picture //
the monochrome picture displayed corretly but the colored one is not clear.
Please if there is any idea to help me I would be very gratefull.
Looking forward to hearing from you..Best Regards
Mariem2011-05-17 4:36 AM
Hi tkjmail,
I'm trying to display images on the LCD screen (ILI9329) using an STM32F103ZET6, the problem that I couldn't display colored pictures, I used the ''LCD_WriteBMP function'' for that and I tried with monochrome pictures and it worked well using the ''LCD_DrawMonoBMP function'' which is provided for displaying monochrome BMPs.(these functions are from the demo's in the STonline) Actually, I convert the images into an hex code using a software called the Hex Workshop then I put the image as a const like this for example: const unsigned char IMAGE[] :{ 0x00, 0xFF, 0xFF, 0x00, 0xFF, 0xFF, 0x00, 0xFF, 0xFF, 0x00, 0xFF, 0xFF, 0x00, 0xFF, 0xFF, 0x00, 0xFF, 0xFF, }; an then in the call of the function : LCD_WriteBMP((u32) IMAGE); // if it's a colored picture //LCD_DrawMonoBMP((u32) IMAGE); // if it's a monochrome picture //
the monochrome picture displayed corretly but the colored one is not clear.
Please if there is any idea to help me I would be very gratefull.
Looking forward to hearing from you..Best Regards
Mariem2011-05-17 4:36 AM
Hi jj.sprague,
I'm trying to display images on the LCD screen (ILI9329) using an STM32F103ZET6, the problem that I couldn't display colored pictures, I used the ''LCD_WriteBMP function'' for that and I tried with monochrome pictures and it worked well using the ''LCD_DrawMonoBMP function'' which is provided for displaying monochrome BMPs.(these functions are from the demo's in the STonline) Actually, I convert the images into an hex code using a software called the Hex Workshop then I put the image as a const like this for example: const unsigned char IMAGE[] :{ 0x00, 0xFF, 0xFF, 0x00, 0xFF, 0xFF, 0x00, 0xFF, 0xFF, 0x00, 0xFF, 0xFF, 0x00, 0xFF, 0xFF, 0x00, 0xFF, 0xFF, }; an then in the call of the function : LCD_WriteBMP((u32) IMAGE); // if it's a colored picture //LCD_DrawMonoBMP((u32) IMAGE); // if it's a monochrome picture //
the monochrome picture displayed corretly but the colored one is not clear.
Please if there is any idea to help me I would be very gratefull.
Looking forward to hearing from you..Best Regards
Mariem2011-05-17 4:36 AM
Hi Mariem.
First I have to say that you don't have to post 3 posts with the same context, this won't speed up the process helping you!
About your problem, I haven't used ST's picture function, as I've made my own. You can check this thread for more information about that code and some errors with it:
https://my.st.com/public/STe2ecommunities/mcu/Lists/ARM%20CortexM3%20STM32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/ARM CortexM3 STM32/Hard Fault error
Best Regards
Thomas Jespersen
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.