2010-01-11 10:09 AM
STM32F103 and WiFi chip
2011-05-17 4:36 AM
Hi.
I'm working on another project which needs a WiFi connection. I've allready got a WiFi chip module from ZeroG Wireless, called ''ZeroG Wireless G2100''. Are there anybody who knows how to control this module with the STM32F103? OBS: I have programmed alot in Basic and C for other uC's (PIC & AVR), but I'm new to the Ride7 enviroment! Best Regards Thomas Jespersen2011-05-17 4:36 AM
Hi! I'm looking for a way to add wireless capability to this processor too.
I found this interesting STM32F103-based device:http://www.seeedstudio.com/depot/micro-digital-storage-oscilloscopedso-nano-p-512.html
which is open-source and schematic is available. If you find any solution, please let me know! Alessandro2011-05-17 4:36 AM
Ok, I will try ;)
2011-05-17 4:36 AM
Quote:
Are there anybody who knows how to control this module with the STM32F103?
The module neither knows nor cares what is being used to control it! You just need to do whatever the Datasheet tells you! Standard procedure for interfacing anything to anything else - irrespective of the specific devices involved - is: See also:2011-05-17 4:36 AM
@apoppi-
You come across as smart/caring STM user - you're certainly trying to assist. Must come to the defense of mon ami ST7 - he is pointing out that poster is a tad ''too quick'' on the trigger - allowing his need/desire to exceed his2011-05-17 4:36 AM
Quote:
On 08-01-2010 at 11:18, Anonymous wrote:Quote:
Are there anybody who knows how to control this module with the STM32F103?
The module neither knows nor cares what is being used to control it! You just need to do whatever the Datasheet tells you! Standard procedure for interfacing anything to anything else - irrespective of the specific devices involved - is: Yes, but you should take into account that maybe one does not have a spare month to reinvent the wheel and write a SPI low level driver then a TCP/IP stack over it from scratch. Better rather focusing on the application. Said that, I suppose that the question from tkjmail was: ''Is there any library or driver or application note for Zero-G modules on STM32 family?'' Ciao!2011-05-17 4:36 AM
The point is that the only parts that will be specific to the STM32 are the parts that deal directly with the STM32's specific features - such as the SPI. And, for those parts, the fact that it's talking to a ZG2100 is irrelevant.
So you can just look at any STM32 SPI examples for that. Similarly, the operation of ZG2100 is independent of what controller is being used - so you can look at generic examples for that. It is really important to understand this, as this is common to pretty much all projects! Understanding this allows you to correctly focus your activities - instead of looking for one unique STM32-specific solution, you can use any generic implementation, and concentrate just on the STM32 specifics. Of course, if you're not really interested in how to do it, but just want an ''out-of-the-box'' solution - then that's a different question!2011-05-17 4:36 AM
I have allready developed a fully working library for the ATMEGA, in Arduino C-language though, so I don't know is I will be able to port that.
But that includes the communication protocol, and a complete TCP/IP protocol too!2011-05-17 4:36 AM
Quote:
I have allready developed a fully working library for the ATMEGA
So, to have done that, you must already be fully aware of how the ZG2100 works. You just need to do the same on the STM32!Quote:
in Arduino C-language though
Is ''Arduino C-language'' really so different from standard, ANSI 'C'?Quote:
I don't know is I will be able to port that.
Why not? Even if you couldn't port it, you could just use it as your model from which to code an STM32 version.Quote:
But that includes the communication protocol, and a complete TCP/IP protocol too!
98% of which will be totally target independent!We’re moving the ST Community to a new platform to give you a better and more reliable community experience.