2009-01-03 8:47 AM
STM32F103 and ILI9320 QTFT display
2011-05-17 4:36 AM
Hi.
I would like to know if any of you have made or got any working code snippets to get started with the ILI9320 connected to a STM32F103? I just finished my project using a Nokia 6610 display with the Epson controller, but as I've got this 2.4'' ILI9320 controlled QTFT display, I want to experiment with that too :) Best Regards Thomas Jespersen2011-05-17 4:36 AM
If not mistaken - that is the TFT ctrl. ic on the STM32 B & E eval boards. Everything you seek should be easily found... (you have truly lucked out)
2011-05-17 4:36 AM
You are right... The code for both of them includes some ILI9320 code, but the STM3210B-EVAL is not parrallel interfacing with the LCD, which the ILI9320 does!
But the STM3210E-EVAL is the right one, just one slightly change... My ILI9320 display is running 8-bit, not 16-bit as the display on the STM3210E-EVAL is doing! Is it possible to change this is the code? And where? :D2011-05-17 4:36 AM
Much depends on how/where your 2.4'' TFT originated. On STM eval kits there are 2 possible pcbs - which hold/connect the TFT. (one for serial SPI, other for 16 bit parallel)
Should you have the TFT supplied by ST - you can ''re-configure'' it to either SPI or parallel input! (can't recall if you can select between 8/16 bits) This is done by re-populating a few smt Rs on the flex pcb exiting the TFT. Tell us the vendor of your 2.4'' - or post spec and we may be able to help further.2011-05-17 4:36 AM
This is the display I've got:
The 8-bit or 16-bit is hardwired on the board, as that is a setting you can choose in the ILI9320 chip!2011-05-17 4:36 AM
Thank you - appears there are just 10 more of that 2.4 TFT - thus ''application review/support'' is hard to justify.
Suggest that you acquire ST's B or E eval board - these have been exhaustively designed to purpose - imho they will save you days/weeks of effort and enable you to properly focus on your application...2011-05-17 4:36 AM
Quote:
Thank you - appears there are just 10 more of that 2.4 TFT - thus ''application review/support'' is hard to justify.
What do you mean by this? I really want to do a project with the QTFT I allready have! :o2011-05-17 4:36 AM
I am simple ST client like you - try to offer support/guidance when/where able - and where it will have the maximum impact/benefit to others.
Believe I've provided a more efficient path for you...2011-05-17 4:36 AM
I think there are many others like me, looking for some ILI9320 8-bit code...
So isn't there a simple step to convert the 16-bit to 8-bit code? I have found every command in the code to be 16-bit, so first of all, they need to be translated, as stated in the datasheet! Also, where in the code is the pins, where the LCD is connected, defined?We’re moving the ST Community to a new platform to give you a better and more reliable community experience.