STM32CubeMonitor (MCUs)

Ask questions on STM32CubeMonitor. Discuss the latest updates, including specialized versions (power, RF, USB-PD).

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMonitor-1.12.0 is available

Hello The version 1.12.0 of STM32CubeMonitor is available on st.com :  https://www.st.com/en/development-tools/stm32cubemonitor.html What are the main changes in this version ? Node-RED® updated to version 4.1.3.STM32 devices list updated.Software de...

STM32CubeMonitor-RF V2.19.0 is available

Hello A new release of STM32CubeMonitor-RF is available on st.com. Click on "Get latest" to download the version 2.19.0. What are the main changes in this version ? Alignment with STM32CubeWB firmware 1.24.0.Alignment with STM32CubeWBA firmware 1.8.0...

STM32Cube Monitor Power buttons issue

Hi everyone.I couldn't find a consistent way to make the buttons "SAVE GRAPH" and "ADD DATALOG" work. They seem to me to be working on a random basis: sometimes yes, sometimes no. Does anybody got the same issue? Does anybody found a way to solve thi...

paolog by Senior
  • 77 Views
  • 0 replies
  • 0 kudos

Resolved! STM32CubeMonitor-Power 1.2.1 installation problem

HiWhen I attempt to install the 1.2.1 version of STM32CubeMonitor-Power on Ubuntu Linux, I encounter a "java.lang.ArrayIndexOutOfBoundsException". I saw some posts about problems with files on the server, but they are quite old, and I have a problem ...

MMotyl by Associate
  • 433 Views
  • 3 replies
  • 1 kudos

STM32CubeMonitor-Power: Add Logarithmic Scaling ?

I have a suggestion for the STM32CubeMonitor-Power application.For the ultra low power applications it would be great if the Y-axis could be logarithmically scaled, so that the area around 0.5-100 µA is more detailed (sleep mode) compared to the acti...

RWalko by Associate III
  • 148 Views
  • 0 replies
  • 0 kudos

Resolved! Probe reports 0 for all monitored variables

On a custom STM32H523-based board connected via STLink 2.0 (swd, p2p in CubeMonitor), all selected variables are plotted as 0, including those whose initial value is not 0. I used the Basic_Flow template, where I set acq_out, acq_in, and loaded varia...

STM32CubeMonitor-1.12.0 is available

Hello The version 1.12.0 of STM32CubeMonitor is available on st.com :  https://www.st.com/en/development-tools/stm32cubemonitor.html What are the main changes in this version ? Node-RED® updated to version 4.1.3.STM32 devices list updated.Software de...