2024-03-01 1:09 AM - edited 2024-03-01 1:11 AM
Hello
I am trying to powerup external 8MHZ crystal on STM32F407VET6 MCU but it is completely dead. I run the LED bliking program using HSI, and it is working sucussfully. Boot 0 and Boot1 pins have been PD with 500 ohm.
I also run the same code to use HSE on STM4 Discovery board after removing R68, I see HSE on board is working.
Below are my caclulation
Frequency = 8 Mhz,
Co = 7 pF ( as per datasheet)
CL= 10 pF ( as per datasheet, used 20pF CL1 and CL2)
ESR = 100 ohm ( as per data sheet)
After calculation gmcrit comes..
gmcrit = .287
gm = 5 ( from ST data sheet)
gain margin = 5/.287 = 17
so gain margin > 5 condition is met.
I also changed Rext to 0, 100, 200, 500 , 1000 ohm. HSE is dead.
PCB design seems ok , and I assume for now no issue with PCB design.
I have gone through AN2867, but not sure what point I am missing.
Kindly suggest where could be the fault. I eliminate software issue as same code is making HSE work on Discovery board.
Solved! Go to Solution.
2024-03-04 1:25 AM
@Peter BENSCH thanks for the reply!
So the LSE is usually the sensitive part, and I understand that for power saving reasons it's high impedance -> low power - but more sensitive
> All in all, it is therefore highly recommended to ensure a super clean layout for the crystals ...
Definitely! Sometimes a little hard for the beginners, but my experience with other ICs is that there were never any problems - even with my first "bad" PCB layouts 25 years ago. ;)
Just saying that the AN sounds as if 3 mm too far away and everything breaks down.
Looking over the HSE / user problems here, most of the time it was a broken component or the caps were far from the recommended values - or not mounted at all.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.