2026-06-04 7:53 PM
We are currently using the NDK crystal NX3225GD 8 MHz (EXS00A-CG04874) for the HSE clock of STM32F412VG and STM32F469BI.
This crystal is also used on evaluation boards, and we understand that it is an approved custom-order part.
However, we are currently facing procurement issues due to long lead times, and this part is not readily available.
As an alternative, we are considering using the standard NDK part NX3225GD 8 MHz (STD-CRA-3), although its specifications differ as shown below:
NX3225GD 8 MHz (EXS00A-CG04874)
NX3225GD 8 MHz (STD-CRA-3)
We understand that the alternative part has lower accuracy and wider temperature variation.
Would it be acceptable to use the NX3225GD 8 MHz (STD-CRA-3) as a replacement for the HSE in these devices?
If there are any concerns (e.g., clock accuracy, USB/communication interfaces, or PLL performance), we would appreciate your advice.
2026-06-05 1:24 AM - edited 2026-06-05 1:34 AM
Hello,
How to select a compatible crystal and load capacitors for STM32 with layout guidelines
AN2867 "Guidelines for oscillator design on STM8AF/AL/S and STM32 MCUs/MPUs"
2026-06-05 2:05 AM
The NX3225GD 8 MHz (EXS00A-CG04874) is actually not difficult to purchase.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.