STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LTDC MIPI-DSI Configuration using stm32H747 and ST7701S

Hi STM community, I have interfaced an st7701s driver IC-based display with stm32h747 chip using MIPI DSI in RGB565 mode and using only the internal SRAM(512KB) of stm32 as the frame buffer(2*480*480 Bytes) but the display framebuffer looks like star...

USB to CAN interface

Hello ST community, I'm working on an interface board based on STM32F412 to send CAN frame from a computer using USB communication. For the moment I'm doing some tests with the CDC stack and the default ST's USB virtual com port driver on Windows 10....

oli_the_true_one_0-1709195364993.png oli_the_true_one_1-1709195591831.png

Resolved! HSE crystal dead

HelloI am trying to powerup external 8MHZ crystal on STM32F407VET6 MCU but it is completely dead. I run the LED bliking program using HSI, and it is working sucussfully. Boot 0 and Boot1 pins have been PD with 500 ohm.  I also run the same code to us...

Nico3_0-1709283992146.png
Nico3 by Senior
  • 10942 Views
  • 20 replies
  • 10 kudos

DCMI OV5640 STM32L4A6

Hi Community!My goal is to capture an bmp image with the resolution of 640x480. But to check first if the camera is correct connected and works perfectly, I'm trying to take a JPEG image.I've successfully connected my Nucleo-L4A6ZG with an Adafruit d...

nicola3 by Associate II
  • 2676 Views
  • 1 replies
  • 0 kudos

NRST low + HSE source gone = system freeze instead of reset

Posted on March 11, 2016 at 03:09I have two chips, a master and a slave, both STM32F429.  The master is using the internal HSI as a PLL clock source.  The master is outputting a 16 MHz signal that the slave is using as a PLL clock source through HSE...

TDK by Super User
  • 2994 Views
  • 9 replies
  • 2 kudos

Resolved! STM32U5 2 MEMS Microphones

Hello, 2 MEMS microphones share a common Clock (PB3, ADF1_CCK0) and Data (PB4, ADF1_SDI0) of a STM32U585QI.Using ADF the PDM signal is processed successfully. It processes either the data of the either falling or rising edge depending on setting Init...

h p by Associate III
  • 2709 Views
  • 2 replies
  • 1 kudos

Using NUCLEO F756ZG - Checking speed of calculations

Hello all,Just started working with STM - Nucleo is my first trial at thisI am operating at 216MHzI noticed this while loop is taking almost 80uSec to complete with the simple trial floating point calculations& output a square wave that I can see on ...

JJAYAR by Associate II
  • 2728 Views
  • 5 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.