cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L031G6U6 - Stop mode I2C back-to-back transactions not working

anton-st
Associate

Hello,

I've got a setup where I put the STM32 into STOP mode, with wake-up on ADDR match on I2C.

SYSCLK is PLL 32 MHz.

APB = 32MHz.

I've configured I2C to use HSI, and enabled STOP_WUCK.

(The I2C uses DMA).

If I enable HSI16KERON then the device responds as normal to back-to-back I2C transactions. 

i.e. if I want to access registers A, B, C. (Write followed by read) This is fine. 

However when this is disabled it seems to only be able to respond to one transaction (i.e. A is fine, B and C are missed). Is this expected behavior? 

If I put a delay of about 20us it also seems to resolve the problem.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.