2024-01-17 2:02 AM
As i state in the title, what is the best way to detect a connection to a console app on a pc?
I want to include a while loop in my program, that stalls the main program until the user establishes a connection and the program proccedes to the super loop.
Is there a function or a variable that detects the conection and returns true or false respectively ?
SHould i try to create a handshake between the two ?
2024-01-17 3:36 AM
See previous answers:
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.