STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

What do these lines of code do: WM8994 Errata Work-Arounds

Hi all,I'm using an STM32F746 Disco board. I'm not sure if the code (below) for this codec came from one of the examples for this board or other disco or nucleo board but it is from an STM32 example or board or github.There are three lines for "WM899...

Rodo by Senior
  • 2611 Views
  • 3 replies
  • 1 kudos

Resolved! STM32C0 bootloader UART pin assignment

Hello,I have a question regarding the bootloader of the STM32C0 (especially the TSSOP 20 version STM32C031F6Px).According to the datasheet and the reference manual, the bootloader can communicate via UART1 and I2C1.The pins it is using are PA9&PA10. ...

akurtj by Associate
  • 2606 Views
  • 2 replies
  • 2 kudos

Cannot build my project

After the cube ide and programmer updated, the debugger broke and this is the message I would get:make: *** No rule to make target 'ENGC 371\project1\file\STM32F429ZITX_FLASH.ld', needed by 'project1.elf'. Stop. what would be the best take? i am usin...

jberdkan by Associate II
  • 1641 Views
  • 2 replies
  • 0 kudos

Resolved! Distinguish between 2 µC (STM32L071CZY6 and STM32L071KZU6)

Hello,we have an electronic with two possible µC as footprint on the PCB.STM32L071CZSTM32L071KZInside the layout it was necessary to route two signals to different GPIOs, thereforewe have a difference in the configuration.We want to avoid a #define t...

SJung.1 by Associate II
  • 2402 Views
  • 4 replies
  • 4 kudos

Resolved! External VREF+ and VREF- for ADC

Hello,I am using NUCLEO-F756ZG. My application is ADC related. I am measuring an analog signal at high sampling rate. Recently, I had a discussion with my team and had an interesting proposal. Our target signal is pretty much guranteed to be within 0...

rakib2023 by Associate III
  • 5951 Views
  • 3 replies
  • 3 kudos

Resolved! overwriting the data registers of the ADC and DAC in STM32G4

On STM32G474, I have a loop where I read ADC values, process them, and write the result to DAC.I am using the dual ADC mode and reading ADC12_COMMON->CDR . I do not care if I read the previous conversion result, in this case, is there a reason to che...

mete by Senior II
  • 1169 Views
  • 1 replies
  • 0 kudos

Resolved! Clock Frequency of L452RE

Hello, I am having a confusion in understanding the Clock Frequencies for STM32L452RE. In the Datasheet its mentioned that "Several prescalers permit to configure the AHB frequency, the high speed APB (APB2) andthe low speed APB (APB1) domains" It al...

Screenshot 2024-01-30 124735.png Screenshot 2024-01-30 123636.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.