cancel
Showing results for 
Search instead for 
Did you mean: 

Distinguish between 2 µC (STM32L071CZY6 and STM32L071KZU6)

SJung.1
Associate II

Hello,

we have an electronic with two possible µC as footprint on the PCB.

STM32L071CZ
STM32L071KZ

Inside the layout it was necessary to route two signals to different GPIOs, therefore
we have a difference in the configuration.

We want to avoid a #define to distinguish between both firmware with different GPIO settings
for these two signals.

Is there any chance to distinguish between these both µC by any register that we can read?

Greetings
Stefan

PS1:
CPUID -> does not work, it doesn't contain information about the package

PS2:
We tried to use 

#define IOUTENA_PIN_49Pin GPIO_PIN_2 // BGA
#define IOUTENA_GPIO_PORT_49Pin GPIOC

#define IOUTENA_PIN_32Pin GPIO_PIN_1 // QFP
#define IOUTENA_GPIO_PORT_32Pin GPIOA
if (IS_GPIO_PIN_AVAILABLE(IOUTENA_GPIO_PORT_49Pin,IOUTENA_PIN_49Pin))
But this doesn't work also. We guess that both packages contain the same Die, therefore 
the GPIO is available on both µC, but NOT connected to a package pin for both packages.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
TDK
Super User

Utilize differences in the schematic to determine which is which. For example, if PA0 is tied to GND on one of the boards, initialize it as input with pullup and read its value. If it's low, you know that's the board where it's tied to ground.

This is not written anywhere but it has worked for me: For pins that exist on one chip but not the other, and that can be driven, you can initialize them as output high and read their value. If it's low, that's the chip where the pin doesn't exist. Not guaranteed, but may work for you.

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

4 REPLIES 4
TDK
Super User

Utilize differences in the schematic to determine which is which. For example, if PA0 is tied to GND on one of the boards, initialize it as input with pullup and read its value. If it's low, you know that's the board where it's tied to ground.

This is not written anywhere but it has worked for me: For pins that exist on one chip but not the other, and that can be driven, you can initialize them as output high and read their value. If it's low, that's the chip where the pin doesn't exist. Not guaranteed, but may work for you.

If you feel a post has answered your question, please click "Accept as Solution".
Andrew Neil
Super User

@SJung.1 wrote:

Inside the layout it was necessary to route two signals to different GPIOs, therefore
we have a difference in the configuration..


As @TDK said, make use of that difference in routing.

If you have a spare pin available, use that to identify the system.

STM32L071CZ = 48/49 pins
STM32L071KZ = 32 pins

So the CZ has 16/17 pins that aren't available on the KZ; they appear to include PC13, PB2, PB10-15 - so you could use any of them as (an) "identity" pin(s) ....

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

@Andrew Neil wrote:


So the CZ has 16/17 pins that aren't available on the KZ; they appear to include PC13, PB2, PB10-15 - so you could use any of them as (an) "identity" pin(s) ....


Yes, that will work, but not on already existing PCBs. We need a firmware solution for existing PCBs,
therefore i wrote "Inside the layout it was necessary to route". Maybe it was not clear enough what i mean.


@TDK wrote:

This is not written anywhere but it has worked for me: For pins that exist on one chip but not the other, and that can be driven, you can initialize them as output high and read their value. If it's low, that's the chip where the pin doesn't exist. Not guaranteed, but may work for you.


I just checked the schematics and in our case the GPIO is on a pullup resistor to 3.3V.
Therefore your solution seems to be the best solution. We will check this and I will report back here.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.