STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

About STM32H7 PLL configuration and precision

Hello,I've got some questions about STM32H753 PLL setting. 1) There are many configurations of M, N and P parameters that give the same output clock. Are there some configurations that are more precise than others (regarding the output clock) ? 2) Th...

Gpeti_0-1706632520977.png Gpeti_1-1706633322855.png Gpeti_2-1706633366734.png
Gpeti by Senior II
  • 6058 Views
  • 7 replies
  • 4 kudos

USART Receive Interrupt

Hopefully this is more of a sensible non-noob question, it relates to interrupt handling, in my case a simple USART receive interrupt. I can see how the CubeMX tool is managing the .c file, its created an interrupt handler, for me to insert my code, ...

I2C Clock line held low by stm32 and not recovered

Hi,Currently, I am facing an issue with STM32 MCU I2C communication.I have facing an I2C timed-out error on the host side while communicating with the MCU I2C continuously.The I2C clock line was held low when the issue occurred, I wasn't able to comm...

ArunyaS by Associate II
  • 4764 Views
  • 3 replies
  • 1 kudos

ADC Accuracy

Dear ST Community, I am currently working with the STM32L433RC board, specifically utilizing its 12-bit ADC. Despite my efforts in writing a simple program, I have encountered accuracy issues with errors exceeding 4.5%, and in some instances, even su...

Nitin24 by Associate
  • 3342 Views
  • 2 replies
  • 1 kudos

How can I use GPIOx_BSRR register?

Hi,I use stm32h743zi nucleo board and I try to GPIOx_BSRR register .This register has two 16 bit registers "BSRRL" and "BSRRH".As I understand BSRRL is used to set bit and then BSRRH is used to reset bit.GPIOB->BSRRL =(1<<0); to set the zero p...

Bilge by Associate III
  • 20376 Views
  • 15 replies
  • 4 kudos

Resolved! SBSFU package not build for stm32f769i discovery board

While i try to build SBSFU package for stm32f769i discovery board package, User App build failed.I am using SBSFU latest package v2.6.2.IDE version : STM32CUBEIDE_1.7.0I got this below errormake allarm-none-eabi-gcc -z max-page-size=1 -o "UserApp.elf...

PR.6 by Associate II
  • 2934 Views
  • 4 replies
  • 0 kudos

Program Upload method in nucleo stm32f103

Hello Everyone I am try to upload my code through stm32f103 necleo debuger or programmer but  have facing one issue for no st link found error I have attached the pic please give the solution .

yugi by Associate II
  • 5516 Views
  • 4 replies
  • 1 kudos

STSW-PFCBIDIR

Hello all,does anybody know the  workload of the STSW-PFCBIDIR's controller when converting AC -> DC ?Is the controller able to do some more expensive calculations (current controlling) and communication tasks (CAN) ?Kind regards !

jhuebler by Associate
  • 810 Views
  • 0 replies
  • 0 kudos

Resolved! PA9 is high voltage level when configured as input pull-down mode

Hello, everyone.    I use STM32L496 on my board, and use PA9 as a GPIO for input, without any external resister.    Software program is based on HAL. I have a sample demo like this:    int main(void)    {        HAL_Init();        BSP_Init();        ...

1.png 2.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.