STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Ethernet : LwIP stm32h735 Memory

Hi,I'm trying to implement an STM32H735 device with LwIP and FreeRTOS. I've been following this documentation: https://community.st.com/t5/stm32-mcus/how-to-create-project-for-stm32h7-with-ethernet-and-lwip-stack/ta-p/49308Although I've managed to re...

HispaEmo by Associate III
  • 5055 Views
  • 8 replies
  • 0 kudos

STM32H7A3RIT6: Product availability

Hello, I don't know whether this is appropriate place to ask, But will STM32H7A3RIT6 or H7B3RIT6 a good choice for projects considering availability? Are these in production to use on new products and trust the availability exists? Thank you! 

Stop 2 WFI, disabling specific interrupt

Hello everyone, I am working on a custom device that is using an stm32 L433. One of its peripherals is set to generate interrupts to wakeup the device from the stop mode, but there are certain instances where I need it to stop for 30 seconds or so an...

sishchuk by Associate
  • 1005 Views
  • 0 replies
  • 0 kudos

MDMA slower than Memcpy and much more noisy

Using STM's MDMA example, I setup a simple loop to transfer an array of 1000 bytes 100 times.The code worked but the MDMA transfer were causing glitches on the VDD rail.I then compared it to memcpy, and to my surprise found that it was around 18% fas...

Robmar by Senior III
  • 4537 Views
  • 7 replies
  • 2 kudos

Resolved! [question] can I disable the nucleo onboard stlink mass-storage?

Posted on December 05, 2014 at 10:05i'v tested the nucleo on arm mbed, very nice. but, when i use the onboard stlink v2.1 to debug my application board, the mbed mass-storeage disk is always pop-up a window. so, can i disable this disk (not by disba...

wan512 by Associate II
  • 3181 Views
  • 3 replies
  • 2 kudos

SMBUS bus busy check

Hi,I have a power management setup with a smart battery, charger Ic and the host msu - all connected on the SMBUS. I am  facing some issues and I doubt that the data on the SMBUS is getting corrupted. The issue is only happening when the MCU tries to...

Luke_abc by Associate III
  • 4667 Views
  • 7 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.