STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32F030F4 with 32K of flash?

Hello! I am experimenting with a STM32F030F4P6. When I connect it to STM32CubeProgrammer via bootoader (UART), there is an info saying the micro has 32Kb of flash, instead of the expected 16Kb for this part.Is it possible that this microcontroller re...

32Kb.PNG
Castelo by Associate II
  • 5484 Views
  • 8 replies
  • 1 kudos

Resolved! UART Rx Buffer

Hi Comunity, I am very new to STM and got some problems on serial UART. I can get data from my serial, but my problem is if the data received is less than the length of the array, the next data received doesn't overwrite the first data. How do I fix ...

BMNanda_2-1708073182034.png BMNanda_4-1708073222310.png
BMNanda by Associate
  • 3126 Views
  • 5 replies
  • 1 kudos

STM32G030 USART and HAL_Delay strange behavior

Hello all, I've recently received a dev board for STM32G030F6 microcontroller and I wanted to make a simple USART test before continuing. I've started the project using STM32 CUBE MX initializing serial port and clock, also, I've retargeted printf as...

Resolved! Cortex M33 fault handlers not being executed

Fault handlers that work on M4 and M7's aren't being executed on an M33.  The Usage Fault I'm creating (via an undefined instruction) appears to be escalated to a Hard Fault.  The Core stops executing instructions before ever reaching a handler.  Is ...

SRM32G030C6T6 : Delay in ADC conversion (Scan mode with DMA)

Folks,I have setup the ADC to operate in scan mode, there are two analog channels to be converted. The CPU is running at 64 MHz and the ADC is running at 32 MHz. I am using the void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef* hadc) to start processin...

BKesh.1 by Associate
  • 2502 Views
  • 3 replies
  • 0 kudos

Resolved! Problem of porting LwIP to STM32H573I-DK

Hi Everyone,I'm trying to port LwIP to STM32H573I-DK and has referenced to:1. GitHub - STMicroelectronics/stm32h5-classic-coremw-apps at v1.0.0 2. GitHub - stm32-hotspot/STM32H7-LwIP-Examples: Ethernet examples using LwIP + FreeRTOS for STM32H7 Disco...

EyckHuang by Associate II
  • 6878 Views
  • 4 replies
  • 0 kudos

About SPI simplex communication.

This question is about SPI simplex communication.Is there any sample code that realizes SPI simplex communication only by register operations?Also, is there any sample code that uses HAL or LL?I would like to know both cases of sending and receiving....

Resolved! Handle Variable Length Transmission over Uart

Hi!I am somewhat unclear on how to handle variable length transmissions using the STM32F4xx HAL. I have looked at other solutions, and suggestions have been made to use HAL_UARTEx_ReceiveToIdle_DMA() or the ISR equivalent.My situation however, involv...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.