STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32F401 reserving flash sector for config

On STM32F401CCU6I'm trying to reserve these 2sectors for user config in gcc linker script:  Sector - Address ini ~ Address end - Size Sector 0 - 0x0800 0000 ~ 0x0800 3FFF - 16 Kbytes Sector 1 - 0x0800 4000 ~ 0x0800 7FFF - 16 Kbytes RESERVE Sector ...

mrx23 by Associate III
  • 3312 Views
  • 4 replies
  • 1 kudos

What to do with unused opamp pins

We want to use the STM32U585QII6Q for a new design, and I want to know what I need to do with the dedicated OPAMP VINM pins on this package. We don't want to use the OPAMPs. Do I leave these dedicated pins floating or should I connect them to GND?I c...

Resolved! STM32F429I-DISC1 debug issue

Hi.I was in the middle of a debug session in a simple application for the STM32F429I-DISC1 in Keil uVision. I disconnected my board from the computer without ending the debugging session. When I reconnected my board, it wasn't detected anymore and it...

jacobvdz by Associate
  • 1384 Views
  • 3 replies
  • 1 kudos

Resolved! How to trigger IRQ on overflow only?

I am trying to configure TIM3 to reset on incoming PWM pulses and call IRQ on overflow, when pulses not coming. The prescaler and ARR are set for 150% of the PWM period. TIM3 in slave reset mode on trigger from CH2 input. MCU is STM32G051F8P.For some...

maple by Associate II
  • 1913 Views
  • 2 replies
  • 0 kudos

STM32U5[Ax] Usb Host Multi-Packet Data Toggling

Hi all, I am not able to fully understand how the DATA0/DATA1 toggling works when performing multi-packets transmissions. For "multi-packet" transmission I mean that the "num_packets" in USB_OTG_HCTSIZ_PKTCNT register is greater than 1, (i.e. I want ...

bluluiss by Associate II
  • 2128 Views
  • 3 replies
  • 0 kudos

Resolved! Automatically entering and exiting bootloader

Is there a way to make STM32Cube Programmer controls a pair of pins in a CH340 or similar USB to TTL converter, to be able to control BOOT0 and NRST pins of an StM32 micro? I would like to make  a simple circuit that permits entering and exiting a bo...

Castelo by Associate II
  • 1895 Views
  • 1 replies
  • 1 kudos

Resolved! STM32H7A3 I2C_CR1 bit NOSTRETCH settings

Currently try to configurate settings for register I2C_CRI. Not sure which value should I set for bit NOSTRETCH. I am using I2C as master. This bit only effected when using I2C as slave. But in manual mention must kept cleared in master mode.  Meanin...

NRAML.1 by Associate II
  • 3163 Views
  • 2 replies
  • 0 kudos

Resolved! High current draw Vbat Bluepill

Hi,This is the first time I am starting a post, sorry in advance if it's not in the correct place.I have a Blue-Pill with original STM32F103C8T6. I have Vbat hooked up to a 0.33 F super cap via 100 ohm. Vdd is connected to V bat with a BAT54C Schottk...

NLHL by Associate
  • 6185 Views
  • 5 replies
  • 3 kudos

MDMA Block transfer only transfers one block

Hi all, i am trying to use MDMA to transfer data from a cyclic ADC-DMA buffermy ADC buffer is of x size and it is cyclic: adc_buffer[x]and i want to transfer its data via MDMA to a larger buffer while its samplingmeaning that after every ADC iteratio...

shahaf321_0-1708006211819.png shahaf321_1-1708006643985.png
shahaf321 by Associate III
  • 1030 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.