STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! HAL_UARTEx_ReceiveToIdle_DMA() timeout

Hi folks,I'm using HAL_UARTEx_ReceiveToIdle_DMA() on STM32L4. If I use minicom and type a few characters, HAL obviously detects an idle state after each single character I typed.I'd like to configure a idle timeout value used in HAL_UARTEx_ReceiveToI...

Lex by Associate III
  • 2513 Views
  • 2 replies
  • 1 kudos

Resolved! Failed to execute MI command load *.elf - NVIC - Error STM32G0B1?

Hello.I encountered strange CubeIDE behavior on a customer board with an STM32G0B1CEU.I've found similar glitches on this forum, but they mostly stemmed from fake HW.I use all original STM from MOUSER.If I enable PWM on TIM4 in MXcube, without NVIC, ...

RinGO by Associate III
  • 5536 Views
  • 3 replies
  • 0 kudos

Resolved! Input capture not detecting square wave

I have built a sine wave to square wave circuit and now want to measure its frequency with the STM. I can see on the oscilloscope that the circuit works, however I can detect neither a rising nor a falling edge with the chip. It is not a problem with...

waves.JPG
Qwyntex by Associate III
  • 6110 Views
  • 11 replies
  • 0 kudos

Resolved! Bus fault Accessing flash

Hi,MCU- STM32H7I get a busfault exception when I read bank2 flash memory. I can read bank1 with no issues. From the flash register SR2, it shows as ECC double bit error. This is new pcb and I can flash the hexfile to bank1 successfully. Even a Jlink ...

andy_long_0-1708033978473.png andy_long_1-1708034440760.png
andy_long by Associate III
  • 4949 Views
  • 7 replies
  • 2 kudos

STM32H7 UART (DMA with IDLE line) unknown length problem

Hello,I am trying to use UART with DMA with IDLE line for unkown length data reception and I am getting the following error:request for member 'NDTR' in something not a structure or union main.cI coded a couple of years ago a HAL_UART_RxCpltCallback(...

Inigo by Associate II
  • 4713 Views
  • 4 replies
  • 2 kudos

Resolved! LWIP with Ethernet Cable Disconnected

I am using a Nucleo-F429ZI with FreeRtos and LWIP. I am having an issue with LWIP when I start with a disconnected Ethernet Cable and then when I connect it back when the firmware is running.I have a thread with the following code. 1 - The gnetif str...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.