STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How do I set correct stdID for CAN-BUS?

Hi! I've seen some tutorials on can communication and notice that each of them use different StdId's. I'm using two nucle-l433rc-p boards, do I need a specific StdId or will any number between  0 and 0x7FF suffice?  

Mr4 by Associate III
  • 2950 Views
  • 1 replies
  • 0 kudos

Resolved! STM32L4R5 using OCTOSPI2 @LQFP100

Is there any chance to use both OCTOSPI (as 2xQSPI) with a LQFP100 package? There is a OCTOSPIM_P2_NCS but no OCTOSPIM_P2_CLK and Multiplexed Mode is not possible (only on P/Q-variants). Thanks in advance! 

Hu44 by Associate
  • 2564 Views
  • 3 replies
  • 0 kudos

Resolved! stm32L4S5, spi pause between 8-bit frames

Hi all,i am performing some 400bytes blocks transferts by SPI, at 16Mhz.I have NSS off, so no CS up/down between frames.From some testing, whatever system clock i set, or whatever spi clock i set, there is a fixed 4us time between 2 consecutive frame...

heisenbug by Associate III
  • 11342 Views
  • 25 replies
  • 5 kudos

Resolved! LDO for STM32H573AII3Q

STM32H573AII3Q is a 169 pin UFBGA SMPS package. Along with SMPS option, does it also have internal LDO for core supply? Can we use internal LDO to supply core voltage for this package?

madhu1 by Associate II
  • 2810 Views
  • 4 replies
  • 2 kudos

STM32G473QET6 Dual Bank/Boot Mode Question

I am having some issues implementing dual bank/boot.I have set up a dummy project starting at base address 0x08000000 for 256k bytes that will turn on a red LEDI have another dummy project starting at base address 0x08040000 for 256k bytes that will ...

kip18 by Associate III
  • 1766 Views
  • 1 replies
  • 0 kudos

Resolved! NUCLEO-L4A6ZG Board/ST-Link not recognized

After about an month, I connected my NUCLEO-L4A6ZG to my PC again. STM32CubeIDE nor the STM32CubeProgrammer can't recognize my board. I already tried different USB ports and different USB cables.When Trying to run a program the Error Message in the I...

stmax_0-1708545446608.png
stmax by Associate II
  • 1797 Views
  • 2 replies
  • 1 kudos

SPI Send (sizeof) too big

Hi, I am wondering if anyone has any experience with HAL SPI as when I try in 16-bit mode to make a single packet of data manually and use (sizeof xxx) it sends 2x data packets to the oscilloscope and when I specify the packet size as "1" I get the c...

PLee.3 by Associate III
  • 4664 Views
  • 6 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.