STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32H750VBT HRTIM not working

I cant make work the HRTIM. I am using the weact board.I tried HRTIM-A and TRTIM-D using the cubeide (latest updated). the first one using "basic HAL" and the second using "Advanced Hal" instructionsTIM5 works so it seems that clock is working.I adde...

Advanced.jpg Basic.jpg Master.jpg
JLope.11 by Associate III
  • 1486 Views
  • 1 replies
  • 0 kudos

Resolved! LPTIM not counting down in encoder mode, always counts up (G071)

I have an STM32G071CBTx with a rotary encoder wired to GPIO pins PB5 + PB7 (LPTIM1_IN1 and LPTIM1_IN2), but for some reason it will never count down no matter which way the encoder is turned.I have checked the encoder waveforms and they are as expect...

JU by Senior
  • 2316 Views
  • 1 replies
  • 0 kudos

TIM Output compare on STM32F407

Good morning community,I am trying to capture output compare unit.Board: STM32F407G Discovery.I configure TIM1 which is 16bit timer on bus1.Reference clock is 12.5Mhz in our case.I am seeing when I run the code only one time interrupt is generated an...

MG1 by Associate II
  • 17574 Views
  • 3 replies
  • 0 kudos

Master Assigning Unique IDs to Slave SPI Devices

Hi,I have successfully setup SPI between a master to many slave STM32F373s.  I include an 8 bit deviceID in the packet header and the master always initiates the request.I am looking for the best way for the master to assign unique device IDs.  I'm c...

LMorr.3 by Senior II
  • 2273 Views
  • 2 replies
  • 0 kudos

CRC Calculation on STM32L072CZ

Hey STM32 Community, I'm currently working on a project involving the STM32L072CZ microcontroller and could use some guidance on CRC calculation procedures. Here's a rundown of what I'm trying to accomplish: I'm downloading a FOTA .bin file in 1024-b...

Deepu joy by Associate II
  • 1828 Views
  • 1 replies
  • 0 kudos

STM32H747i j-tag debugging

Hello everyone, I am currently working on the SMT32H747i_DISCO board and I was wondering if it is possible to use the Segger J-Link debugger on the Board. There is a j-tag pin out connected to the Dev board which suggests that it should be possible. ...

Resolved! FDCAN g431 doesn't filter

Hello, i'm testing FDCAN in my stm32g431 and it doesn't work well. Messeges goes throught it, even if ID doesn't match (TxHeader.Identifier = 0x102 shouldn't pass, but it does!) static void MX_FDCAN1_Init(void){hfdcan1.Instance = FDCAN1;hfdcan1.Init....

Tomuello by Associate II
  • 2411 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.