STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Oscillator Selection for STM32G4

Hello Community,I am slightly confused while selecting the external high-precision Clock source for our application that uses STM32G474RxT3 series MCUs. I want to use DSC1001DL2-024.0000T as I have these in our inventory, I checked for the operating ...

Chubs by Senior
  • 8388 Views
  • 7 replies
  • 4 kudos

FATFS on STM32L071CB

stm32l071CB flash only 128kB, can fatfs run on Stm32L071CB? Roughly how much space it takes up?The FATFS I used to use on the stm32F103VE platform took up about 200KB of flash because of several large arrays。

屏幕截图 2024-03-25 091714.png
LOMO by Associate III
  • 836 Views
  • 0 replies
  • 0 kudos

Ethernet phy crystal oscillator in STM32H7xxI-EVAL

HiI design a board based on the STM32H7xxI-EVAL, the ethernet PHY is LAN8742A-CZ-TR and according to its the datasheet the crystal specification the drive level need to be 300uW but the maximum drive of X53T-C20SSA-25.000MHz level is only 100uW.Did y...

IMor.1 by Associate II
  • 3632 Views
  • 2 replies
  • 0 kudos

STM32F303 Comparator & ADC for AC RMS measurements

I come from the PJRC Teensy 4.x after many years playing around with it and building a product or two based on it. (NXP IMXRT chip)But for a new project I need to be able to rapidly calculate the RMS value of an AC sine wave from an audio signal, wit...

DResn.1 by Associate II
  • 4259 Views
  • 6 replies
  • 0 kudos

STM32F3 CAN Bus example using HAL Library

Posted on December 20, 2017 at 18:49Hello,I'm trying to bring up the CAN bus on the STM23F303RE nucleo board and am having some difficulty determining which way to go.  I've been unable to find a HAL library example for this platform.  Can anyone po...

Resolved! Changed a few #define -> cube IDE goes nuts.

How in the world is this happening now? Just made some changes there. Renamed and changed the values.The first line has "missing whitespace after the macro name" Aprilfools day is still not here yet!  

Tobe by Senior III
  • 1874 Views
  • 3 replies
  • 1 kudos

GENERATE PWM using ADC values

if (HAL_GPIO_ReadPin(USER_Btn_GPIO_Port, USER_Btn_Pin)){HAL_GPIO_WritePin(TIGGER_GPIO_Port, TIGGER_Pin, GPIO_PIN_SET);HAL_ADC_Start_IT(&hadc1);HAL_TIM_PWM_Start_DMA(&htim1, TIM_CHANNEL_1,(uint32_t*) pwmData1, 300);HAL_GPIO_WritePin(TIGGER_GPIO_Port, ...

Resolved! How many GPIO pins can be used on H563ZI

I am a new user of H563ZI, and I have read the datasheet. I wonder if all pins that can be viewed in cubeIDE can be used as a GPIO pin?For example, as mentioned in the datasheet, PB2 is used as QSPI_CK when solder bridge configurations are not change...

hchienti_0-1711242665854.png
hchienti by Associate II
  • 2841 Views
  • 3 replies
  • 2 kudos

STM32H7 osKernelStart faults to HardFault handler

Hi AllI am working on a data logger code. It is basic at the moment.1, set a an ISRTimmer for 1sec.2, When ISR triggered i set DataLoggerFlag.3, Next loop thru main() i test DataLoggerFlag, if set go to a function and read A0, A1 ports and store back...

oskernalStartError.png
DaveBy2 by Associate
  • 1322 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.