STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

CONFUSION IN USART BLOCK DIAGRAM

Hi, I have a confusion between these 2 USART Block diagram. Figure 1 and Figure 2.Figure 1 shows that the flow of the RX is from RX ENDEC block -> RDR -> Receiver control.Figure 2 shows that the flow of the RX is from RX ENDEC block -> Receive shift ...

1.JPG 2.JPG
WM_IR by Senior
  • 1890 Views
  • 2 replies
  • 0 kudos

P-L496G-CELL02 use the plastic SIM

Hi, we struggle to get P-L496G-CELL02 up and running with a plastic SIM. I know that set pin Sim_select0 to LOW to select the plastic SIM. However, I don't know what software to use and how to set it up. I am a beginner in embedded development. In ad...

harold_f by Associate
  • 775 Views
  • 0 replies
  • 0 kudos

Resolved! STM32F303VCT - Code hangs on sysTick IRQ enable

STM32F303VCTSTM32CubeIDE 1.14.1Simple program generation with IDE, main() while loop user code that toggles a GPIO.System hangs during HAL_Init() for the sysTick vector in: void HAL_NVIC_EnableIRQ(IRQn_Type IRQn){/* Check the parameters */assert_para...

jlag by Associate III
  • 6934 Views
  • 16 replies
  • 5 kudos

Resolved! STM32F303VCT - Applicatoin code not running outside of STMCubeIDE.

STM32F303 - Application running fine in CubeIDE debugger, custom board. It will not start as standalone, programmed with CubeIDE or CubeProgrammer with .elf or .hex.I have created an 'attach' run debug configuration, which can successfully display pr...

jlag_1-1709927450108.png jlag_0-1709927405306.png jlag_2-1709927661693.png
jlag by Associate III
  • 11446 Views
  • 10 replies
  • 4 kudos

Stm32f446re with E22t900d

Firstly, hello, I currently have the Nucleo-F446RE and E22t-900d LoRa module. First of all, how do I connect these two products? Then, how can I send the data I receive via the stm32 card to another LoRa module connected to the USB port of my compute...

gazili by Associate
  • 781 Views
  • 0 replies
  • 0 kudos

Resolved! STM32F7 and STM32H7 HDMI implementation

Hello,Please forgive me for what is probably a newbie question.  What is required to implement an HDMI interface with the STM32F7 or H7 MCU series?  Is a DSI-to-HDMI bridge always required?  What is the max. supported display resolution?Thanks,Scott

Resolved! Does NUCLEO-IKS01A1 support I3C? (with NUCLEO-H503RB)

Hi, I'm trying to check I3C protocol with NUCLEO-H503RB and IKS01A1.I just followed below link for I3C. https://wiki.st.com/stm32mcu/wiki/Getting_started_with_I3CAnd I can see that the master transmit the data but there is no ACK from the slave.(I've...

Resolved! STM32 RTC3 Mixed Mode: Writing TR resets SSR?

RTC3 of some newer STM32s introduce a RTC mixed mode, where both binary part (32-bit down-counting sub-seconds register SSR) and classic BCD calender (TR/DT) mode are operational.In my case I am using this for classic style BCD alarms together with b...

Resolved! FDCAN Bootloader for STM32G0B

I did not find any solution of Bootloader for CAN2.0A or CAN2.0B with SMT32. Currently i am using below part no. MCU-'STM32G0B1CCT6' CAN IC-'ISO1044BD'

Pooja321 by Associate II
  • 4433 Views
  • 7 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.