2024-01-24 2:55 AM - edited 2024-01-24 4:11 AM
Hopefully someone can help.
Below I get some connection and identification proceeding, but it fails at the end with
"Cannot identify target as an STM32G0/G4/L4/L4+/L5/U5/WB/WL family device."
UPDATE!: I copied the openocd.exe from my installation of stm32CubeIde and it works.
Although there is a STM32U5x.cfg added to the latest openocd on the official build, there must be something missing from the binary, which I can fix by using the STM32CubeIde openocd.exe
Original Problem
Open On-Chip Debugger 0.12.0 (2023-01-14-23:37)
Licensed under GNU GPL v2
For bug reports, read
http://openocd.org/doc/doxygen/bugs.html
Info : auto-selecting first available session transport "hla_swd". To override use 'transport select <transport>'.
Info : The selected transport took over low-level target control. The results might differ compared to plain JTAG/SWD
Warn : The selected adapter does not support debugging this device in secure mode
Info : clock speed 500 kHz
Info : STLINK V3J10M3 (API v3) VID:PID 0483:374E
Info : Target voltage: 1.796388
Info : [stm32u5x.cpu] Cortex-M33 r0p4 processor detected
Info : [stm32u5x.cpu] target has 8 breakpoints, 4 watchpoints
Info : starting gdb server for stm32u5x.cpu on 3333
Info : Listening on port 3333 for gdb connections
Info : Unable to match requested speed 480 kHz, using 200 kHz
Info : Unable to match requested speed 480 kHz, using 200 kHz
CPU in Non-Secure state
[stm32u5x.cpu] halted due to debug-request, current mode: Thread
xPSR: 0xf9000000 pc: 0x0808a8ac msp: 0x20043250
Info : Unable to match requested speed 4000 kHz, using 3300 kHz
Info : Unable to match requested speed 4000 kHz, using 3300 kHz
** Programming Started **
Warn : Cannot identify target as an STM32G0/G4/L4/L4+/L5/U5/WB/WL family device.
C:\nf-interpreter\EXEC : error : auto_probe failed
embedded:startup.tcl:1516: Error: ** Programming Failed **
in procedure 'program'
in procedure 'program_error' called at file "embedded:startup.tcl", line 1581
at file "embedded:startup.tcl", line 1516
2024-03-29 5:20 AM
Hi @TerryFogg ,
Thanks for coming back with the solution you found. I suggest you repeat the solution in a new reply that you mark as a solution.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.