STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to configure STM32F103 USB endpoints.

Been reading thru the F103 datasheet to try and figure out why my TinyUSB based code isn't working. The datasheet says.. "For mono-directional/single-buffer endpoints, a single register can be used to implement two distinct endpoints". The F103 has...

Bags by Associate III
  • 2333 Views
  • 9 replies
  • 2 kudos

Resolved! FreeRTOS vs TIMER interrupt task

Good days at all. I need to start a project and I'm unsure which path to take: I'd like to create an application that requires some tasks to run in parallel and some to run at different times. I've used timers as interrupts in the past, so as soon as...

SMusc.1 by Senior
  • 1091 Views
  • 2 replies
  • 2 kudos

Resolved! MTBF: STM32H743VIT6

We have used STM32H743VIT6 in our project. To calculate product life cycle we required below details,MTBFFITUsage temp (°C)Confidence Level (%)Activation energy (eV)Test temp (°C)Test duration (hours)Sample sizeFails 

nisha851 by Associate
  • 305 Views
  • 1 replies
  • 1 kudos

Resolved! Stm32H7 CAN bus communication issue

Hello I am having an weird issue and was hoping if someone could provide some guidance. Hardware : Two Stm32 H7 with CAN TranscieverNvidia OrinCan Adapter/Sniffer (Canable) What works :  Stm32H7 to Stm32H7 Nucleo Board Can Bus works.Nviia Orin < - > ...

Amogh by Associate III
  • 19845 Views
  • 19 replies
  • 9 kudos

Resolved! STM32H7 FDCAN configured in CAN2.0 is not working

Hi guys i have a nucleo h7A3Zi-q dev board . i am trying to receive CAN messges sent from ESP32 borads . esp is sending can  frame by using SN65HVD232D. and i configured the FDCAN to receive the can messages . esp can is set at 500 kbits , and my stm...

b1aze_0-1765963936905.png b1aze_1-1765963951279.png
b1aze by Associate III
  • 1432 Views
  • 6 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.