STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Could UART function on lines with 10nF capacitance?

I am using all of the pins of a STM32L471RE in a design.In manufacturing, there is the need to communicate with the MCU over UART (during Functional Testing (FCT)). The problem is that all the pins are taken, so there are no free UART ports available...

uart_setup.png
oscarw by Associate II
  • 3416 Views
  • 4 replies
  • 4 kudos

Ho to add own piece of code in to the make file?

It's possible to add my own piece of code to the make file? I'm asking because I've already tried to add it, but after clicking the "Build" button, my code disappears!PS - I want to add "Generate packed filesystem for serving Web UI".

DK.7 by Senior
  • 1895 Views
  • 1 replies
  • 1 kudos

Custom usb

Hi Team, I'm using STM32H743 series controller.I want to implement USB Base class on STM32H743. Unfortunately CubeMX will not support it.Any example code which works on Base class- 00h, Sub class -00h and protocol -00h

RJ1 by Associate
  • 1771 Views
  • 2 replies
  • 1 kudos

Resolved! STM32G050C8T6 ADC_IN11: inconsistency in the datasheet?

Hello,According to the datasheet PB7 can be used as  ADC_IN11.Is this an error in datasheet? ADC_IN11 is already used by PB10 and cubeMX doesn't seem to allow me to use PB7 or to remap this pin. How can I use ADC_IN11 on pin PB7 as mentioned in datas...

AHame_0-1712593418190.png
AHame by Associate III
  • 7876 Views
  • 12 replies
  • 10 kudos

STM32H747I JPEG DecodeDMA

Hi all,I´m new to STM32 and just recently bought an STM32H747I-DISCO. I needed one with a touch screen for a project. I was going thru the examples and got the LCD DSI SingleBuffer to work but was having problems with the JPEGDecodeFromFLASH DMA. I u...

JL3 by Associate
  • 1004 Views
  • 1 replies
  • 0 kudos

STM32L4A6 reading OK but writing failed "error erase memory"

Hi everyone,I'm getting stucked with a programming issue.I try to load a HEX file into a STM32L4A6 chip on a BMS board.I've checked the wiring of the st-link/v2 programmer and everything is OK.The chip can be read from the CUBE software but when i wa...

pierrew by Associate II
  • 1533 Views
  • 3 replies
  • 0 kudos

IEC60335 SelfTestLib

In our legacy STM32f103 project a ST library named "Self Test Library" is used. It has version 1.0, dated 10/01/2007. That library is certified according to IEC60335. I found it in an archive named IEC60335.zip, but I have no idea if that's the origi...

Resolved! STM32H723 Internal Temperature Measurement vs. Ambient

All:Setup - STM32H723 with VREFP = 3.00 VI have connected internal temperature to ADC3, and I am able to display degrees C on "Live Expressions". With VREFP set to 3.00 V, I am seeing lower readings than ambient. Using __HAL_ADC_CALC_TEMPERATURE( ), ...

ToddA by Associate II
  • 3263 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.