STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Getting speaker to work with STM32F3discovery

Hi,Following the code from https://github.com/antoinevg/stm32f3-rust-examplesAnd my speaker is not making any noise when GND and PA04 connected. I have one of these https://www.jaycar.co.nz/27mm-all-purpose-replacement-speaker/p/AS3002Specifications:...

bibble235 by Associate III
  • 957 Views
  • 0 replies
  • 0 kudos

STM32F103VB contain PFAS substance or no

Dear Sir / Madam,Would you please help to check does STM32F103VB contain PFAS substance or not?If No, please provide the PFAS free declaration.If Yes, please provide the CAS number contain Fluorine substance. Thank you. 

NG by Associate
  • 900 Views
  • 0 replies
  • 0 kudos

STM32H743 and ST7701S compatible problem

Hi,Itˊs my first time programing on ST,there are some questiions i want to ask for advice:1.Does STM32H743 and ST7701S compatible?2.Which IDE should I use?STM32cubeIDE or vscode platform which is easier for beginner to use ?or other IDE?3.Can i use A...

Resolved! How to implement IAP(Ymodem Protocol) on DualCore(h745)?

I'm tring implement IAP on NUCLEO-H745ZI-Q.So. I seen STM32h743-eval IAP Example.But I have two bank and two core for cm7 and cm4.I don't know how to implement the bootloader.And should I create and transfer bin files for cm4 and cm7 respectively?

Circuit diagram & schematic request

Hi,Note: circuit diagram & schematic requested ,Preferably in altium designer(mjlrprecision@gmail.com)New to the electronics, doing small projects,For our project we made Free-fall detection board using STM32G030F6P6 & Lis2Dh, it is working fine dete...

Jan58 by Associate
  • 1947 Views
  • 2 replies
  • 1 kudos

Resolved! Portenta H7 Development with STM32CubeIDE

I'm looking for some instructions on how to develop firmware for the Portenta H7 using the Portenta Breakout Board with the STM32CubeIDE. Before ST Microelectronics comes back and says they can't help because the H7 is not their product, that is unac...

rtalan by Associate III
  • 10712 Views
  • 7 replies
  • 5 kudos

STM32WL to microSD Card FR_NO_FILESYSTEM Error Help.

Hello All, I will attach my PCB Layout as well as IOC file screenshot for reference. I am using this tutorial https://01001000.xyz/2020-08-09-Tutorial-STM32CubeIDE-SD-card/.I got it working on a nucleo board, but am transitioning over to the PCB now....

Screenshot 2024-04-23 at 1.46.16 PM.png Screenshot 2024-04-23 at 1.42.40 PM.png Screenshot 2024-04-23 at 1.43.02 PM.png
jflaxman by Associate II
  • 1148 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.