STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

internal temperature tamper not triggering

hii am using stm32u585 controller for my project . here i enabled the internal tamper detection using the below code  /* USER CODE BEGIN TAMP_Init 2 */ sAllTamper_inter.IntTamper = RTC_INT_TAMPER_1|RTC_INT_TAMPER_2|RTC_INT_TAMPER_3|RTC_INT_TAMPER_9;...

sabari1_0-1767359791489.png sabari1_1-1767359949290.png
sabari1 by Associate III
  • 458 Views
  • 2 replies
  • 0 kudos

Resolved! STM32H723 - ULPI and pc2_c/pc3_c

Hi all,I'm currently designing a board that requires using an stm32h723 with USB HS (I need more bandwidth than FS allows). The stm32h723 I'm using doesn't expose pc2 or pc3, which are needed for ULPI DIR and NXT respectively. Instead, pc2_c and pc3_...

sophie by Associate II
  • 1030 Views
  • 5 replies
  • 0 kudos

Nucleo H7S34L8 ADC Configuration

Hello,   I am very heravily struggling setting up my ADC in continmous conversion mode with HPDMA with multipkle channels.   The DMA seems to stay idle, while the SFRs are saying the ADC is running.   Is there a issue in the config of the ADCs?   /* ...

Vidar by Associate III
  • 472 Views
  • 2 replies
  • 0 kudos

Resolved! Untimely wakeup during WFE on stm32g431.

I have a project in which I try to sync my assembly code on a signal on a GPIO, using WFE for minimum latency and jitter.I use a Rust HAL ony for initialisation of the clock and to put some GPIOs into input mode, and one in output mode that I use to ...

treguy by Associate II
  • 577 Views
  • 3 replies
  • 1 kudos

STM32G474CEU6 with 1.8V supply

 Hi, The STM32G474CEU6 LQFPN48 was previously used in our projects with a 3.3 V supply, where we successfully operated a 25 MHz FL2500326 crystal using 6.8 pF load capacitors, and the crystal oscillation was stable.In the current design, the same con...

How to use arm_rfft_q15 properly.

I created a 10Hz sine function with phase of pi/4, amplitude of 1000, bias of 2000, a sampling rate of 1kHz, and 2048 samples (20 periods in total) and saved it into q15_t input[2048].I created a fft stract by arm_rfft_init_q15(&S, 2048, 0, 0)I enter...

0693W00000HrDsAQAV.png 0693W00000HrDs5QAF.png 0693W00000HrDrMQAV.png
RBen-.1 by Associate
  • 3102 Views
  • 2 replies
  • 0 kudos

Resolved! DMA not working along with ADC

Tried running DMA with ADC simultaneously by configuring both in CubeMX, but I am not getting correct ADC values in the buffer. The sin wave from the signal generator is completely distorted. The ADC works individually without the DMA by filling the ...

alien1 by Associate
  • 579 Views
  • 4 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.