STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Data transfer from SAI to DTCM using HPDMA not working

I am using a Nucleo-N657X0-Q board to prototype a data collection system that collects samples from an ADC connected to the SAI peripheral and places the results in RAM. If I use CPU AXI RAM0 as the destination this works correctly, but if I change t...

nige_w by Associate
  • 596 Views
  • 1 replies
  • 0 kudos

bootloader with 2 application

 I am working with an STM32F0 device and I want to implement a firmware update mechanism.My current plan is to split the internal flash into three regions:Bootloader: 0x08000000Application Slot 1 (App1): 0x08004000Application Slot 2 (App2): 0x0800800...

scotzap by Associate II
  • 873 Views
  • 5 replies
  • 3 kudos

STM32N6 power supply simplification

I am working on an STM32N6 hardware design, and have reviewed both development kit reference designs (MB1939/MB1940). Both designs use the same power supply scheme, when using internal SMPS it has 2x 3V3 regulators and 3x 1V8 regulators.I am interest...

Resolved! RCC_CR.HSEBYP not reset by Software Reset

Experimenting with STM32F427 and STM32F446 I found out, that the RCC_CR.HSEBYP bit is *not* reset by Software reset. It is reset only by NRST and Power-On reset.While applications where this could lead to problems (i.e. where HSE clock source is chan...

STM32H725ZGT6 Full Bridge Converter with TIM1 or TIM8

Hello I would like to build a full bridge converter according to attached topology picture. The signals for controlling the switches should be like in the picture pwm_scheme. The frequency should be 500KHz. How to configure TIM1 or TIM8 on STM32H725Z...

smal by Associate
  • 406 Views
  • 0 replies
  • 0 kudos

Resolved! STM32H562 - 5V Tolerant Pins Derating Impact

Hello Community,We are currently evaluating the STM32H562IGT6 microcontroller for our development project. During our review of the device’s pinout, we observed that several GPIO pins are designated as FT (5‑V tolerant). We would like to request clar...

RajeshM by Associate II
  • 394 Views
  • 2 replies
  • 0 kudos

Resolved! STM32H562/3: clarify the max frequencies in DS14258 rev6

According to the STM32 datasheet, the maximum clock frequency of TIM6 and TIM17 is shown as 64 MHz, while that of TIM1 to TIM8 is shown as 200 MHz. There is a conflict in the documentation, so please confirm which one is correct. (DS14258 Rev6,page 1...

Adu_It by Associate
  • 667 Views
  • 2 replies
  • 1 kudos

Resolved! USBX issue in the STM32N657X0H3Q (Nucleo-N657x0-Q) board

  We are working on a bare-metal application using USBX on an STM32N657X0H3Q device.In CubeMX, we configured USB1_OTG_HS under Connectivity and enabled USBX in Middleware. However, when we execute the following function: static void MX_USB1_OTG_HS_P...

image.jpg
Grace_04 by Associate III
  • 863 Views
  • 3 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.