STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Tranceiving & Receiving Data with UART on STM32H735G-DK

Dear all,I've been wrestling with a communication glitch that's been causing me some serious headaches. Here's the lowdown: I've got this control board hooked up to a pump, and I've been trying to send commands to it via USART1 on my own STM32H735G-D...

Resolved! STM32F4 SPI high level 5V

Sorry, I have another question to ask everyone. I'm currently using the Nucleo F429ZI with SPI interface to receive 12-bit encoded data from another ADC. The Vdrive of that ADC can provide 3.3V or 5V for driving. However, the high level of the STM32F...

Scarlet_0-1713766357977.png
Scarlet by Associate III
  • 16055 Views
  • 28 replies
  • 14 kudos

STM32F405 ULPI USB3343

Hello Guys,I am new to STM and USB HS but have some experience with PICs and other AVRs. I've designed my own custom board (for a keyboard). So after I generated the USB HID code with STM32cube IDE, I successfully downloaded it to the STM, however, n...

maubla by Associate
  • 1891 Views
  • 2 replies
  • 1 kudos

NOR Flash(external memory )- Status error

Hi all, I'm working on the NOR Flash via OSPI(using as QSPI) with the STM32U585 board. implementing this via filex and levelx, i have done all the configuration referring to the example provided by ST with the minor changes. I'm getting error in the ...

meghasb by Senior
  • 1743 Views
  • 1 replies
  • 1 kudos

Working with STM32 is so frustrating

This morning I got an email from ST which included a section on using VS Code to target STM32 CubeMX projects.This appeals to me since the STM32CubeIDE is seriously lacking in focus from ST. It has looooooong standing bugs which no-one cares about, b...

KMill by Senior II
  • 1706 Views
  • 2 replies
  • 2 kudos

USB project example

Hello,I need very simple communication of my STM32F722RET6 via USB (Full Speed) - I need to send every 10 ms only data of 20 bytes to some program made by C# in Visual Studio. I found some samples of USB communication on GitHub but I was not able to ...

Timer callback issue?

Hi,I have timer with period 1 sec (80 MHz clock):  htim2.Init.Prescaler = 80-1; htim2.Init.CounterMode = TIM_COUNTERMODE_UP; htim2.Init.Period = 1000000-1;  Global var (volatile uint32_t) increased every time counter wraps around void HAL_TIM_PeriodE...

Lex by Associate III
  • 2048 Views
  • 3 replies
  • 1 kudos

Resolved! STM32H503EBY uart bootloader

Hello! The AN2606 manual does not describe which pins of STM32H503EBY UART1 uses.STM32H503EBY have WLCS25 package, but i found information only for others packagesOn SO8, WLCSP18, TSSOP20, and UFQFN28 packages USART1 PA9/PA10 IOs areremapped on PA11/...

EAlek.3 by Associate
  • 1262 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.