STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STML496ZGT6P

Can anyone face this issue at STM32CubeMX tool while generating the code. 

sag_0-1714125523019.png
sag by Associate III
  • 1212 Views
  • 1 replies
  • 0 kudos

Resolved! Seeking Advice for Communication on Nucleo-h743zi2 Board

Hello,   I'm currently controlling a motor with the nucleo-h743zi2 board.   I'm sending commands to the motor driver via PWM and reading the encoder's values. I can currently send commands from a PC and receive encoder values through UART communicati...

HMsDobby2 by Associate III
  • 1977 Views
  • 2 replies
  • 1 kudos

GPIO read correct data

Hi there ! I start a project with STM32G031k8. This board i'm gonna make is  a RS485 slave on the pin 4-5-6-7 of GPIOA i put a dipswitch with pullup resistor , and i read in this way: uint16_t Add = ( 0x00F0 & GPIOA->IDR)>> 4 ;  right now my add is 5...

SGian.1 by Senior
  • 2224 Views
  • 2 replies
  • 0 kudos

How to connect microsd card in stm32f407

Hii, I was trying to connect microsd card module with stm32, i was unable to connect with it because the SDIO interface was not available at stm32f407 discovery board. also it support spi communication but not getting how to get with it. can some one...

Shubham08 by Associate III
  • 5118 Views
  • 7 replies
  • 1 kudos

STM32G491RE QUADSPI ISSUE

Hello,I'm facing a strange issue with the quadspi peripheral.I'm using it to interface with a W25q256jveiq, a quad spi enabled flash chip from Winbond.As long as I use one line SPI or dual I/O mode all works fine.I can access the flash chip with no i...

zeboss49 by Associate III
  • 2612 Views
  • 4 replies
  • 0 kudos

Resolved! Single USB Host to Multiple USB Virtual Ports

Hello,I have an STM32F373 and have successfully enabled a USB virtual com port.I currently send data packets from a PC host to the slave device and include a 'deviceId' in the packet data header.I would  like to support the single PC host communicati...

LMorr.3 by Senior II
  • 8117 Views
  • 9 replies
  • 1 kudos

STM32F103RCT6烧毁

早上好! 在装机生产中STM32F103RCT6芯片能正常工作,成品机器交付客户使用后出现STM32F103RCT6芯片烧毁损坏的情况。成品机器与客户端通讯接口内信号线是直接连接芯片I/O口,客户端与成品机器联合使用,当成品机器出线异常(后排查为STM32F103RCT6芯片烧毁),客户端未出现芯片烧毁的情况。相关直连引脚为【PB3】&【PB4】,PB3做输出I/O量,PB4做输入I/O量。 请问该芯片烧毁的原因可能是哪些?

YANG_3 by Associate
  • 1580 Views
  • 1 replies
  • 0 kudos

Resolved! Write/Read issues with HyperRAM S70KL1282 on OctoSPI2 (STM32H7A3)

I am currently ramping up a new project which has a HyperRAM installed (S70KL1282 - like in the example project of STM32H735G). With the help of this sample project code I can successfully write and read with memory mapped mode from the 16 MB RAM - b...

GS1 by Senior III
  • 3399 Views
  • 4 replies
  • 2 kudos

Resolved! USB-OTG- USB Device Problem

HI STM Team,I am new to STM32 Board. I am using NUCLEO-F439ZI Board. When I was connecting my USB-OTG side to my PC, I will suffer from the "Unknow USB Device" Error, The error screenshot was attached below for your reference . Please Guide me to rec...

Ramachandran1992_1-1714037120515.png

Resolved! STM32F4 Series a Question About I2S

Hi, I am trying to do an application where I am using 2 PDM output digital MEMS microphones to get a stereo sound from them and then play it. My question is when I select I2S as Full-Duplex Master for STM32F407VG it only has 1 SD pin. Should connect ...

mdmrl00 by Associate II
  • 2484 Views
  • 3 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.