2024-04-25 7:32 AM
Hello Guys,
I am new to STM and USB HS but have some experience with PICs and other AVRs. I've designed my own custom board (for a keyboard). So after I generated the USB HID code with STM32cube IDE, I successfully downloaded it to the STM, however, nothing happens. No USB device is detected by the host (PC).
Am I missing something? Do I have to program somehow the USB3343? Is there anything I have to add to my code to use ULPI?Is it the known bug with STM32f405 and USB3300? (clock configs should be good, same with layout, soldering etc..)
I haven't right now an osci acessible... However during debugging all the USB regs. seemed to be 0.
Anyone expereince with STM and ULPI?
Thank's!
2024-04-25 9:13 AM
Dear @maubla ,
Welcome in our STCommunity and pleased to help with our members . I have a question, why using ULPI for High speed device ? and not using our embedded PHY for full speed devices , HID Keyboard do not need High speed communication. if possible to share your schematics or used board to help and assist at software code.
We provide built-in examples also ready to use when running our default Development Kits : Nucleo or Discovery kit.
Let us know.
STOne-32.
2024-04-25 9:36 AM
hello, thanks for your fast reply.
I am basically using HS ULPI with an external PHY for personal challenging reasons, & yes I know HS isnt required for HID Keyboard devices.
During debugging I saw today that the STM32 doesnt even start initializing the USB. An error already occurs during Clock Init: (external clock is a 16Mhz crystal)
Please let me know if you knowt anything.

if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.