STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

no indication on the display

Hello,what do I have to change in the code so that I see something on the oled display 0x78?Maybe someone has a tip for meThanks :)...#define ssd1306_I2C_Port hi2c2#define ssd1306_I2C_ADDR 0x78...#define ssd1306_WIDTH 128#define ssd1306_HEIGHT 64...I...

SPI_Receiving data is improper because of HAL Functions

I am sending multiple bytes in spi protocol. The sender is sending properly through AARDWARK(Total Phase Control)Software. But only the odd number of bytes are received and the receiving is not proper using these HAL_Functions. What is the issue?int ...

Resolved! SPI_multiple_bytes_transfer

I am sending multiple bytes in spi protocol. The sender is sending properly through AARDWARK(Total Phase Control)Software. But only the odd number of bytes are received and the receiving is not proper using these HAL_Functions. What is the issue?chec...

Resolved! STM32G474VET3: DAC output and comparator input question

As i am using inside comparators. For that i can see below available options for reference voltages. My question is about DAC output can it be set internally or i have to make physical connection by DAC out put pin to comparator input  

sag_0-1714040226057.png
sag by Associate III
  • 2055 Views
  • 2 replies
  • 0 kudos

Resolved! STM32 Nucelo F429ZI, LWIP a simple application not working

Hello everyone,  I have been trying to run a simple LWIP application on my STM32 F429ZI board. I can see the LED green and orange of the Ethernet jack (CN14) are on which indicates the link is up and running. but no luck with pinging the board from m...

Regarding issue with NUCLEO-F429ZI.

NUCELO-F429ZI Encountered a issue.When i connect a USB ,it is showing like FAIL and a message is shown on the screen likeThe interface firmware FAILED to reset/halt the target MCU.Can any one let me know what is the reason for this and solution for t...

MCU 150C

I have been developing a system using an SMT32L476 but it is only rated to 125C .I'm looking for a temperature range of 150C .  Its is desing into a piece of test equipment that goes within a thermal Chamber and cna overshoot ot 130-50 before settlin...

SSSL by Associate II
  • 1790 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.