2024-04-24 11:35 PM
Hello,
I need very simple communication of my STM32F722RET6 via USB (Full Speed) - I need to send every 10 ms only data of 20 bytes to some program made by C# in Visual Studio. I found some samples of USB communication on GitHub but I was not able to communicate (in best case without making some special drivers) with C# program. Only VCP worked but the program was in contiuous cycle to read COM port. Please can you advice me where I can find some working sample of connection STM32 and program via USB?
Thank you
2024-04-25 7:31 AM
Here is examples for F722 Nucleo board STM32CubeF7/Projects/STM32F722ZE-Nucleo/Applications/USB_Device at master · STMicroelectronics/STM32CubeF7 · GitHub
In your case, REPORT_COUNT should be at least 0x14 to send 20bytes of data. Make sure to configure your timer to interrupt every 10 ms.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.