2026-01-05 4:03 PM
I am working on an STM32N6 hardware design, and have reviewed both development kit reference designs (MB1939/MB1940). Both designs use the same power supply scheme, when using internal SMPS it has 2x 3V3 regulators and 3x 1V8 regulators.
I am interested in combining several power supplies if possible, notably:
1. Is it possible to tie all 3V3 together?
While AN5967 suggests to apply VDD33USB in the last step of power sequencing, the VDD33USB supply is noted to be independent of the other supplies within the N6, just like the VDDIOx supplies. The reference designs have tied VDDIO4 to VDD at 3.3V, which makes me believe I could also combine VDD33USB and VDD.
Aside from just VDD33USB and VDD, all the 3.3V peripherals on the dev kits come from the second 3V3 supply, can I tie all peripheral 3V3 to VDD33USB and VDD, so I have a single 3V3 rail on the PCB?
If not what about the STM32N6 disallows this?
2. Can I combine 1V8 for peripherals with VDD18AON?
Is there anything against connecting 1V8 for flash and ram and such with VDD18AON? since my VDDIO for those IO banks will be tied to VDD18AON anyways.
Overall, the power sequencing diagram only shows that VDD/VDDA18AON must be stable before VDDCORE, but it does not show any sort of required ramp time for the other supplies. Can I simply have a single 3V3 and 1V8 supply that ramp up, then VDDCORE comes up automatically afterwards?
2026-01-06 5:39 AM
Hello @aroberts-figure
Yes, this is possible, but under the condition that you respect the explanations above.
For powering an STM32N6, the design we recommend is as follows:
Always present:
Note 1: Here VDDIO2 + VDDIO3 = 3.3V for external memory at low-frequency data rate.
Enabled with PWR_ON:
Note 2: Here VDDIO2 + VDDIO3 = 1.8V for external memory at high-frequency data rate.
Note 3: In external SMPS mode, VDDSMPS and VDDA18PMU can be connected to GND (internal SMPS is not used).
At minimum, we recommend:
In External SMPS mode:
2 voltage regulators (LDO or DC/DC Buck) at 1.8V (VDDA18AON direct and VDDA18 enabled by PWR_ON)
Internal SMPS:
I hope it will help you.
Best regards,
Romain,
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.