2026-01-06 3:05 AM
Hello sir/miss ,
According to the STM32H7 datasheet, the range of the HSE external crystal oscillator is 4M - 48MHz. However, when we used the STM32H7IIT6-EVAL evaluation board and replaced the original 25MHz surface mount passive crystal oscillator with a 48MHz passive crystal oscillator, we were unable to obtain the corresponding 48MHz frequency from the MCO-PA8 pin.
Summary: All conventional passive crystals from 4M to 40MHz were tried and worked fine. However, for external passive crystals above 40MHz , just like 48MHz, the MCO output waveform frequency was 16MHz, which is 1/3 of the HSE frequency, and it was unable to output 48MHz.
Please provide a solution or suggest areas where we can improve the test. Thank you very much!
2026-01-06 3:11 AM
You chose a crystal that works in 3rd overtone mode.
Be sure to select one that works in fundamental mode:
2026-01-06 3:11 AM
Hello,
@shaunSHAUN wrote:
Summary: All conventional passive crystals from 4M to 40MHz were tried and worked fine. However, for external passive crystals above 40MHz , just like 48MHz, the MCO output waveform frequency was 16MHz, which is 1/3 of the HSE frequency, and it was unable to output 48MHz.
From this statement I suspect a failing HSE oscillation startup.
So when you replaced that crystal, did you check if that crystal is compatible with STM32?
Please read this article: How to select a compatible crystal and load capacitors for STM32 with layout guidelines
+ Refer to the application note AN2867 "Guidelines for oscillator design on STM8AF/AL/S and STM32 MCUs/MPUs"
2026-01-06 3:12 AM
HI,
so for the "48MHz" crystal you picked a third overtone type, that will its fundamental resonate at 16M.
1. try with a crystal thats in fundamental mode or a crystal oscillator (+ HSE bypass setting)
2. why try/using crystal at the given limits ? Never a good idea... Better to stay in middle of possible range.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.