2026-01-04 6:08 PM - last edited on 2026-01-05 9:04 AM by Andrew Neil
Solved! Go to Solution.
2026-01-05 12:19 AM - edited 2026-01-05 12:56 AM
Hello,
1) This is a known issue raised already by another customer. There is a typo regarding the maximum allowed clock frequencies for TIM16 and TIM17. The 64 MHz applies to TIM12 and TIM15 when HSI_KER_CK/1024, HSI_KER_CK/8, and CSI_KER_CK/128 are selected for input capture; otherwise, it is 250 MHz for all timers in VOS0. To avoid confusion, the 64 MHz value will be removed from the DS table. It will be fixed in the coming rev of the datasheet. (internal ticket number 221378)
2) The datasheet is always the reference so for the second question I suggest to open a new thread in STM32CubeMx forum board.
2026-01-05 12:19 AM - edited 2026-01-05 12:56 AM
Hello,
1) This is a known issue raised already by another customer. There is a typo regarding the maximum allowed clock frequencies for TIM16 and TIM17. The 64 MHz applies to TIM12 and TIM15 when HSI_KER_CK/1024, HSI_KER_CK/8, and CSI_KER_CK/128 are selected for input capture; otherwise, it is 250 MHz for all timers in VOS0. To avoid confusion, the 64 MHz value will be removed from the DS table. It will be fixed in the coming rev of the datasheet. (internal ticket number 221378)
2) The datasheet is always the reference so for the second question I suggest to open a new thread in STM32CubeMx forum board.
2026-01-05 4:58 PM
Thank you for your helpful response. This has resolved my questions.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.