STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I cant get continuous Data from Sensors with I2C

The MCU I use is stm32f103c8t6 and the sensor is mpu-9255 on the board, there are 5 sensors and I show these sensor values on the LCD screen. I connected a button and when I press the button it moves to the next sensor. The problem is that I want to ...

Broos by Associate II
  • 3463 Views
  • 5 replies
  • 0 kudos

How to compile arm_math.h source in STM32CubeIDE?

Hello All,     I am trying to include arm_math.h for STM32F401RE project, I have all the source file of math.h However when I try to build it. I am getting multiple defination  error at linking stage.Can anyone suggest me how to solve this? I am not ...

NNada1_0-1715784456438.png
NNada.1 by Associate II
  • 3557 Views
  • 5 replies
  • 0 kudos

Resolved! STM32 Ethernet/IP

Does anyone have experience with Etherner/IP on STM32? (STM MCU or MPU are just fine)We are looking for Ethernet/IP example on STM32 but seems not found any thing yet.All we found are just : I-NUCLEO-NETX - netSHIELD industrial ethernet protocols exp...

Dat Tran by Senior II
  • 4221 Views
  • 3 replies
  • 0 kudos

How to unlock RDP level 1 on a STM32U0k8

Hi,I am working on a project using an STM32U031K8U6.I have been experimenting with various low power modes and somehow, It appears that I have accidentally set RDP level 1 protection.I have been using STM32CubeIDE to create and build code and then I ...

JFP by Associate II
  • 3198 Views
  • 3 replies
  • 0 kudos

Resolved! STMG474RE USB FS implementation

Hi together,i´m trying to set up a communication via usb using the usb cdc class to communicate with additional software via a virtual com port running on a local pc using the Nucleo G474RE board.However i can't find a sufficient documentation what i...

j_ic_0-1715774325310.png j_ic_1-1715774344179.png j_ic_2-1715774369039.png j_ic_3-1715774395021.png
j_ic by Associate
  • 1560 Views
  • 1 replies
  • 1 kudos

Resolved! STM32F767 SDMMC DMA read missing first 16 bytes

My ongoing difficulties running FATFS on an SD card has uncovered a problem! A read of the boot sector does not read all the data correctly, specifically the first 16 bytes are all zero. This means that FATFS reports there is no filesystem. The code ...

0693W0000059nS7QAI.png 0693W0000059nSCQAY.png

I2C NOT WORKING

Hello everyone,I'm coming back to you regarding a synchronization problem between master and slave in I2C.I'm making an I2C/UART debug interface, what I want to do is display a menu in a terminal-> When we receive an address from the master (sent in ...

Gojo by Associate III
  • 3036 Views
  • 2 replies
  • 1 kudos

STM32F779 "Package Data Register" always returns the same

Hello, RM0410 says: Spoiler45.3 Package data registerBase address: 0x1FFF 7BF0Address offset: 0x00Read only = 0xXXXX where X is factory-programmedBits 15:11 Reserved, must be kept at reset value.Bits 10:8 PGK[2:0]: Package type0x111: STM32F767 and ST...

Maximum allowed voltage on STM32H755XIH3 adc pin

Hello Team, we are using the STM32H755XIH3 for our new development. in the datasheet there it mentioned the maximum allowed voltage on input pin is 4V. somewhere its mentioned that the allowed voltage is of 3.6V.please let us know what will be the ma...

JYada1_0-1714733198198.png
JYada.1 by Associate II
  • 4607 Views
  • 7 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.