STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

The Usage of source code files after SPL2LL conversion

Dear all,After converting the source code files from SPL to LL. I cannot see any project files in the destination folder. Can these source code files be used by either IAR or STM32cubeIDE? Or do I need to do some configuration first?Thank you.

khwuuk by Associate III
  • 1418 Views
  • 2 replies
  • 0 kudos

SPL2LL converter error message

Dear all,I am trying to convert the SPL to LL using the SPL2LL converter. After pressing the migrate button, I got the message below. Please help. Is it the problem that I chose the wrong directory? I chose the directory where the main.c file is loca...

khwuuk_1-1715615219213.png
khwuuk by Associate III
  • 5872 Views
  • 15 replies
  • 4 kudos

SPL2LL conversion results

Dear all, After the SPL2LL conversion, I got the messages below.Message 1:     [WARNING] -- Line 2096 -- "NVIC_SetVectorTable" No LL API, StdPeriph legacy API is used instead (legacy library) Message 2:[WARNING] -- Line 238 -- "I2C_CheckEvent" No LL ...

khwuuk by Associate III
  • 1092 Views
  • 1 replies
  • 0 kudos

Resolved! BSP Audio STM32F756G- DISCO

Hello, I am trying to play wav audio files from and sd card. The reading of the data works fine but the BSP_AUDIO_OUT_Play doesnt work, It get stuck inside the Dafult handler infinite loop.     

F15javi_1-1714211145939.png
F15javi by Associate
  • 4319 Views
  • 4 replies
  • 4 kudos

Resolved! Use of external oscillator input

Hi i am using STM32G474VET3 controller having below clock input range– 4 to 48 MHz crystal oscillator i am using 16 MHz right now. What is the significance if i use 32 MHz crystal or increase my crystal value. Does it increase speed for instruction e...

sag by Associate III
  • 1610 Views
  • 1 replies
  • 0 kudos

STM32-L432KC CAN mailboxes are not emptied HAL_CAN_ERROR_PARAM

Trying to send a CAN message every second but after a few tries it returns the HAL_CAN_ERROR_PARAM error. Tried to check if there is an empty mailbox available before sending the next can message but the mailboxes arent emptied. Main.c is below, the ...

oguh by Associate II
  • 1879 Views
  • 2 replies
  • 1 kudos

Flash 5 click_STM32H50B Disco

I am working with the NAND Flash 5 Click module, the STMOD+, and the STM32H750B Disco board. My goal is to read, write, and erase data in this memory. However, I cannot find the necessary drivers for this memory. Who could help me or has an example o...

Resolved! FW crashes randomly after hours - how to debug?

This is not a question, it is more an "experience report", related to find "reliability issues" (flaws) in my FW.Many people know: there is a HardFault_Handler: called when something goes wrong (e.g. accessing a not-existing memory address, e.g. addr...

tjaekel by Lead
  • 3476 Views
  • 4 replies
  • 9 kudos

Display Upgradation.

I found an Oscilloscope project (https://www.youtube.com/watch?v=sSbzYbYM4iM) but I want to make the display larger. I currently have a 2.8 TFT SPI 240x320 v1.1 Display (Vcc, Gnd, Reser, DC, SDI[MOSI], Sck, Led, SDO[MISO]), and I want to use it as a ...

blue-pill.jpg 2.8 TFT Dislay (Touch).jpg
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.