STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Hard Fault detected

HiI am using STM32U575ZIT6 microcontroller. I have created a simple program that turns on several LEDs on the board, but when switching to the non-secure zone, a Hard Fault occurs.

Resolved! STM MCUs: how to sync Audio IN and OUT?

This is more an experience report.I want to get audio from an INput source and forward to an OUTput sink. And both should stay in sync "forever" (I do not want to have a clock drift, I do not want to have the condition to skip a sample or to add one,...

scope_timing.png
tjaekel by Lead
  • 2221 Views
  • 1 replies
  • 0 kudos

Resolved! STM32U5xx: ADF as PDM MIC input - mono and DC offset?

Using STM32U5A5 MCU and adding the ADF example (taken from en.stm32cubeu5-v1-4-0\STM32Cube_FW_U5_V1.4.0\Projects\STM32U575I-EV\Examples\MDF\ADF_AudioRecorder) seems to work.I have changed to use the PLL3 and setup 3,072MHz as PDM MIC CLK (for 48KHz s...

STM32U5A5_ADF_PDM.png
tjaekel by Lead
  • 3240 Views
  • 2 replies
  • 1 kudos

Resolved! STM32F412 Multiple PWM Control Inquiry

I am developing a product using the STM32F412REFxLQFP64 chip, and I want to implement multi-PWM control. For TIM2 buzzer control: TIM_HandleTypeDef TIM2 PB10 ------> TIM2_CH3 TIM3 is used to generate a 1kHz waveform: TIM_HandleTypeDef TIM3 Channel 4 ...

KOPRO by Associate III
  • 5290 Views
  • 10 replies
  • 1 kudos

STM32H7 ADC characteristics

Hi,I'm working on a setup with a filter and some electronics to get an analog signal ready for a ST microcontroller (STM32H723VG). I want to simulate everything, even the part inside the microcontroller that handles the signal. But the problem is, I ...

STM32H723VG datasheet.png STM32H7.png
HKet by Associate II
  • 3287 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.