STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! 'F3 COMPxMODE[1:0] discrepancy

So, which is correct and which is wrong?The same is in RM313 for 'F37x.Would those who wrote/modified AN4232 pay more attention to checking the facts through actually writing test cases, rather than applying the "modern feel and look", this must have...

0690X00000DBuRlQAL.png

Resolved! [STM32H750XBH6] Output current Question

Hello,I use STM32H750XBH6, DataSheet 'Absolute maximum ratings' say that 'Output current sunk by Px_C pins' is 1mAWhat does Px C mean? Does it mean all the pins of GPIOC?Or something else? Thanks!

微信截图_20240524114156.jpg
Passerby by Associate III
  • 2176 Views
  • 3 replies
  • 2 kudos

Problem receiving the data through UART using DMA

Hi, I am using STM32F407 board to communicate with a serial device. I have been using HAL_UART_Transmit() to send the data and using HAL_UART_Receive_DMA() to receive the data. Part of the code is shown below. After every receive command I am suppose...

FR_Invalid_Object error - STM32L4R5ZI Nucleo Board

I am currently trying to get an SD card working with SPI on an STM32L4R5ZI Nucleo board, using STM32CubeIDE V1.13.2 using the latest L4 embedded package. I currently have my code opening the card and even opening the file (I receive FR_OK for both, e...

JayDev by Senior II
  • 6004 Views
  • 7 replies
  • 3 kudos

input capture direct mode from remap

While setting up input capture for the stm32h743 using the IOC.  On timer 2 channel 4, I have pin conflicts, but the IOC gave me the option to use "input capture direct mode from remap".  I can not find a description of what remap means.

Leroy3 by Associate II
  • 2108 Views
  • 1 replies
  • 0 kudos

Regarding distortions at pins of IC

We are using STM32H743IIK6 microcontroller. When using analog pins(ANA) to receive analog input signals, will their be interference effect if the two pins are next to each other? 

AkshayMR by Associate II
  • 828 Views
  • 0 replies
  • 0 kudos

Resolved! CORDIC q1.31 to integer conversion

Hello everyone. I want to understand the CORDIC engine, using the nucleo-u575zi board. The guide says that the cordic uses data in q1.31 format. Could please someone explain how to convert results into an ordinary int value? And how to convert an int...

Skfir by Senior
  • 5739 Views
  • 3 replies
  • 3 kudos

unable to program an external nand flash memory

hi guys,I hope this message finds you well.I am currently working with the STM32H743Eval2 evaluation board with an external nand flash memory "Micron MT29F2G16ABAEAWP" , and i'm trying to run the code provided in the firmware  on the same memory but ...

Hamxa10_0-1716415940943.png Hamxa10_1-1716416002982.png Messenger_creation_f45f8ea7-0fb3-4f3d-94bd-897e01a21d92.jpeg Messenger_creation_4e3905d7-bd75-4c15-9503-340e8db34fee.jpeg
Hamxa10 by Associate
  • 2235 Views
  • 2 replies
  • 0 kudos

COM port drop out

I have a written C# windows application that receive data continuously from MCP2221A. MCP2221A receive data from STM32 UART through receive data line. When the laptop goes for sleep (in battery mode), it send a suspend signal (it will go low) to the ...

cjaya.2 by Associate II
  • 1599 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.