STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Regarding ANA pins of STM microcontrollers

We are using STM32H743IIK6 microcontroller. There are analog only pins, designated as ANA. What is the use of these pins? Also, what will be the difference when GPIO is used for analog functionality and ANA pins are used for the same purpose? 

AkshayMR by Associate II
  • 1893 Views
  • 2 replies
  • 1 kudos

Resolved! STM32H5 DCMI maximum input data size

Hi.I want to acquire data from a 5M pixel image sensor (for example OV5640) with YCbCr4:2:2, 8bit using DCMI.(I want to process the image data, so I need to transfer it to memory using DMA)However, AN5020 and RM0481 (Rev1) mention a maximum of 2048*2...

AN5020.png
BLUE by Associate
  • 1564 Views
  • 1 replies
  • 0 kudos

STM32G491 Pin1 Marking

Hey, i got this STM32G491MET6The datasheet does not really help here to identify pin 1, since there are 4 markings to see. Anyone has a clue on this? In the previous revision of this datasheet, Pin 1 is bottom left . Already burnt 2 mcus because of t...

TwixMeow by Associate
  • 7747 Views
  • 9 replies
  • 6 kudos

Resolved! stm32h745 disco

Hello, i bought this board and the board was burned with sw with signal genrator and other things. Somone can send me the .HEX file that i can burned it again? i cant found this file.

Resolved! Bootup Delay on STM32F446

Hello,I am running simple LED Blinking on STM32F446RE.I want to measure the Bootup Delay once it is Hard Reset.I have conducted the following test through Oscilloscope and Logic Analyzer.I want to know and prove this through calculation.Is there any ...

Nibesh by Associate II
  • 1334 Views
  • 1 replies
  • 0 kudos

Resolved! Using ADC1 and ADC3 with DMA and timer

Hello everybody!I am using STM32F429 as my central controller for a project. I need to read 20 ADCs and process the signals by the 10 kHz sampling-time. I am using 14 channels of ADC1 and 6 channel of ADC3. Before, I have done it for one ADC when I u...

Resolved! ADC on Nucleo 401RE

Hello everyone, im trying to understand how the configuration and the use of the ADC is usued on a NUCLEO401RE. I've read the datasheet and reference Manuel but still its not clear.I have configure the pin A0 on CubeIDE to be an ADC input. But now i ...

willow by Associate III
  • 5055 Views
  • 9 replies
  • 5 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.