STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H573I-DK_aws_ri_tz certificate

I'm working with the stm32h573i-dk kit and I need a connection to AWS. I performed the step-by-step procedure as described in the webinar https://content.st.com/stm32h5-connects-smart-things-in-a-secure-way.html, however, I got stuck at the end, wher...

ffjunq_2-1712689414514.png
ffjunq by Associate III
  • 4048 Views
  • 3 replies
  • 0 kudos

Resolved! STM32F303VC clock setup with crystal on OSC_IN

We have custom HW with an STM32F303VC processor.There is a 12 MHz crystal with an 18pF in parallel wired to OSC_IN and OSC_OUT.The power budget is basically unlimited so we would like to run the device as fast as possible with this configuration.Peri...

jlag_0-1716560475207.png jlag_2-1716560572625.png
jlag by Associate III
  • 1514 Views
  • 1 replies
  • 1 kudos

STM32F4 Timer Counter Never Starts Counting

Hi, I am attempting to enable TIM1 to act as my program's tick timebase as SysTick is being utilized by the FreeRTOS kernel to generate PendSV interrupts. I configured this in CubeMX (Timebase set to TIM1) but I cannot get TIM1 to start ticking. Atta...

notTicking.png
Elliott99 by Associate II
  • 2345 Views
  • 4 replies
  • 0 kudos

SerialPort with registers

Hello, I am trying to do one simple task with my STM32 board using just registers and interruptions in USART2.Basically I have to wait until I receive data via serialPort, then activate interruption that should increment the value of my data by 1. Af...

summ98 by Associate
  • 854 Views
  • 1 replies
  • 0 kudos

Resolved! No BSDL Files for STM32H7RS

The BSDL files for STM32H7RS do not contain files for STM32H7RS.Is the JTAG command length the same for STM32H7RS as for other STM32?

STM32F4 Timer DMA requests

Hello Team,I am using the STM32F469NIH6 to implement a timer triggered DMA and I need some clarity on a few points here-I see that that there are three possible requests possible for a timer triggered DMA. I understand that the TIM8_UP is to trigger ...

Jansunil_0-1716460451673.png
Jansunil by Associate II
  • 3426 Views
  • 5 replies
  • 0 kudos

Resolved! Program won't run after upload

I have designed my own PCB and I have the problem that while the code uploads successfully, it doesn't run.I have checked NRST and BOOT0 and both should not be the problem. I have found a similar issue where the chip didn't get a clock signal and the...

Qwyntex_0-1716384046463.png
Qwyntex by Associate III
  • 12744 Views
  • 22 replies
  • 3 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.